IMX6Q Sabrelite board Linux 3.10.17_1.0.0_ga PCIe issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q Sabrelite board Linux 3.10.17_1.0.0_ga PCIe issue

712 Views
paullalthuamsan
Contributor I

Linux 3.10.17_1.0.0_ga bootup on IMX6sabrelite board with PCIe adaptor from boundary device. I connect Broadcom WiFi Bluetooth PCIe chipset. I boot the device, PCIe device is detected once, but then PCIe device are never listed again with lspci command. I tried with other PCie device and other IMX6Q board, reset multiple times, lspci never list my device.

Its the first time I work with PCIe, not much knowledge about it.

Do any one face this type of issue. Pls suggest any solution

Labels (3)
0 Kudos
Reply
1 Reply

506 Views
igorpadykov
NXP Employee
NXP Employee

Hi Paul

one can try attached patch and check below link

PCIe link doesn't come up with XIO2001 PCI bridge on iMX6Q custom board

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply