Dear Sir
I want to ask you about the MCIMX6Q-SDB.
Customer purchased the evaluation board.
(700-27516 REV B / SCH 27516 REV C4)
It bundles the SD card written Android 4.2.2.
It freeze at the "Freeing init memory" when it boots with the SD card.
Please refer to the attached file(Android_4.2.2_error log.txt).
I also confirmed the startup operation with Android 4.4.2_1.0.0.
It freezes similarly at "Freeing init memory".
Please refer to the attached file(Android_4.4.2_1.0.0_error log.txt).
Q1.
Is there a report of startup failure with combination of Android 4.x.x and IMX6Q-SDB(700-27516 REV B)?
Q2.
I think that it is the initial failure of the hard.
Is there anything else to check before requesting RMR?
Best Regards,
Eishi SHIBUSAWA
Original Attachment has been moved to: Android_4.4.2_1.0.0_error-log.txt.zip
Original Attachment has been moved to: Android_4.2.2_error-log.txt.zip