IMX6Q-SABRE Board does not boot due to eMMC file system corruption

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6Q-SABRE Board does not boot due to eMMC file system corruption

2,027 Views
nagarajan-r
Contributor I

Hi,

My i.MX6 SABRE board does not boot due to corrupted file system in eMMC.

Below are the configuration details.

Board - i.MX6 SABRE board

Processor : i.MX6 Dual Core A9 processor

OS : QNX 6.6 RTOS

Boot options : eMMC ,SD card and USB

The Board was working fine and it suddenly does not boot after power-up, it stops with the below error message in the QNX IPL program and did not proceed further.

Welcome to QNX Neutrino Initial Program Loader for Freescale i.MX6Q Sabre-Smart (ARM Cortex-A9 MPCore)
copy_named_file_fat32 failed!
BPB signature is wrong
error detecting BPB type
load bmp failed.
boot select=eMMC

I've tried with booting from SD card by placing the ipl-imx6q-sabresmart and QNX-IFS files in a bootable SD card.

In this case,  it did not print any of the above debug statements in the serial terminal. I've changed the boot option switch from eMMC -> SD card.

Can anyone please let me know, why it does not detect the SD card and how to resolve this issue.

Attached the serial terminal debug message snapshot.

Thanks

Nagaraj

Labels (1)
0 Kudos
Reply
2 Replies

2,019 Views
igorpadykov
NXP Employee
NXP Employee

Hi Nagarajan

 

for this issue it is necessary to reflash emmc image anew, since nxp does not support qnx

may be recommended to applly for help to vendor of that qnx software.

 

Best regards
igor

0 Kudos
Reply

2,007 Views
nagarajan-r
Contributor I
Hi igor, Thanks for your response. Since we are not able to access SD card,we are not able to access eMMC, we couldn't format/reflash the eMMC. I will check with QNX team support. thanks Nagaraj
0 Kudos
Reply