IMX6Q通过RMII接口与以太网交换机芯片KSZ8895RQXCA相连,设备树中关于网络的配置如下:
&fec {
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_enet>;
phy-mode = "rmii";
phy-reset-gpios = <&gpio1 18 0>;
fsl,magic-packet;
status = "okay";
fixed-link {
speed = <100>;
full-duplex;
pause;
};
};
pinctrl_enet: enetgrp {
fsl,pins = <
MX6QDL_PAD_ENET_MDIO__ENET_MDIO 0x1b0b0
MX6QDL_PAD_ENET_MDC__ENET_MDC 0x1b0b0
MX6QDL_PAD_ENET_TX_EN__ENET_TX_EN 0x1b0b0
MX6QDL_PAD_ENET_TXD0__ENET_TX_DATA0 0x1b018
MX6QDL_PAD_ENET_TXD1__ENET_TX_DATA1 0x1b018
MX6QDL_PAD_ENET_RX_ER__ENET_RX_ER 0x1b0b0
MX6QDL_PAD_ENET_RXD0__ENET_RX_DATA0 0x1b018
MX6QDL_PAD_ENET_RXD1__ENET_RX_DATA1 0x1b018
MX6QDL_PAD_GPIO_16__ENET_REF_CLK 0x4001b0a8
MX6QDL_PAD_ENET_CRS_DV__ENET_RX_EN 0x1b0b0
>;
};
目前:imx6q(192.168.1.4)无法ping通同一网段内的我的电脑(192.168.1.2),我的电脑也无法ping通imx6q。通过示波器可以看到imx6q上的TX0/TX1/RX0/RX1都有信号,而且MX6QDL_PAD_GPIO_16__ENET_REF_CLK上有50Mhz的信号。在我的电脑端使用Wireshark抓包工具可以看到imx6q发送的数据包,而且此时我的电脑也响应了该数据包,但是imx6q端没有接收到数据包,也可能是接收的是错误的数据包。
1、使用imx6q(192.168.1.4)ping我的电脑(192.168.1.2)的信息如下:
root@imx6qsabresd:~# ping 192.168.1.2
PING 192.168.1.2 (192.168.1.2) 56(84) bytes of data.
From 192.168.1.4 icmp_seq=1 Destination Host Unreachable
From 192.168.1.4 icmp_seq=2 Destination Host Unreachable
From 192.168.1.4 icmp_seq=3 Destination Host Unreachable
From 192.168.1.4 icmp_seq=4 Destination Host Unreachable
2、使用 ifconfig eth0命令查看的信息如下:
root@imx6qsabresd:~# ifconfig eth0
eth0 Link encap:Ethernet HWaddr 32:34:46:78:9a:dc
inet addr:192.168.1.4 Bcast:192.168.1.255 Mask:255.255.255.0
inet6 addr: fe80::3034:46ff:fe78:9adc/64 Scope:Link
UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1
RX packets:0 errors:2562 dropped:0 overruns:0 frame:2562
TX packets:573 errors:0 dropped:0 overruns:0 carrier:0
collisions:0 txqueuelen:1000
RX bytes:0 (0.0 B) TX bytes:311879 (304.5 KiB)