U-Boot 2018.03-dirty (Feb 11 2022 - 18:53:49 +0530)
CPU: Freescale i.MX6Q rev1.3 at 792MHz
CPU: Industrial temperature grade (-40C to 105C) at 20C
Reset cause: POR
Model: Freescale i.MX6 Quad SABRE Smart Device Board
Board: Custom-Board
DRAM: 2 GiB
board_init() called setup_fec() calledpower_init_board() begin
PMIC: PFUZE100! common_init
i2c_idle_bus: failed to clear bus, sda=1 scl=0
PMIC: PFUZE100 RET =0x-16
PMIC: PFUZE100! DEV_ID=0xffffffda REV_ID=0xffffffda
pfuze_common_init() done == 0
No device returned from pfuze_common_init initcall sequence 8ffa510c failed at call 17804d3c (err=-19)
### ERROR ### Please RESET the board ###
IMX6Q : PMIC pfuze is pointing to pfuze100 but Giving some random number as device id i.e DEV_ID=-38 instead 0x10.
Let me know how to change the pmic
You can refer to the method https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/Porting-PF1510-in-i-MX6ULL/ta-p/1253948
@nxp ,
Any update on this issue?