IMX6Q I2C Open drain IBIS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6Q I2C Open drain IBIS

1,571件の閲覧回数
barakbarak
Contributor I

HI,

Please provide CSI0_DAT8 IBIS model for OPEN DRAIN IO buffer on the imx6q platfrom.

Thanks!

ラベル(2)
0 件の賞賛
返信
1 返信

1,442件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Barak

ibis model is available on

IBIS Model (1)
i.MX 6Quad and i.MX 6Dual IBIS File
i.MX6Q|i.MX 6Quad Processors|Quad Core|NXP 

however there is no special open drain characteristics.

So one can simulate waveform high to low transition with existing ibis model

(working low transistor in data buffer) and use rc model for low to high transition

as high transistor is turned off.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信