IMX6Q DDR3-1866使用压力测试工具测试失败

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6Q DDR3-1866使用压力测试工具测试失败

6,194 次查看
yz_z
Contributor III

大家好,

      请问一下各位,有用过DDR3-1866在IMX6Q上的吗?我最近在imx6q板子上使用DDR3-1866的时候,使用压力测试工具V2.8进行校准失败。

1、采用I.MX6DQSDL DDR3 Script Aid V0.10.xlsx进行配置,根据DDR3 calibration for MT41K256M16TW-107 帖子上Artur Petukhov 员工说的“For Data Rate options of 1600 and faster use the 1600 value.”进行配置。然后校准失败。而后尝试根据IMX6DQRM.pdf手册进行修改相应配置参数,均失败。

2、同样一块PCB板子,就是DDR3不同型号,如果是DDR3-1600的话,使用压力测试工具进行校准和压力测试,在396MHz~635MHz之间均可以通过测试。而DDR3-1866却不行。

       哪位可以指点一下,使用DDR3-1866时,该如何进行配置.inc脚本文件?谢谢!

标签 (1)
标记 (1)
0 项奖励
回复
4 回复数

4,389 次查看
yz_z
Contributor III

      在社区内,关注DDR3-1866的使用问题时,发现这个帖子i.MX6DQSDL DDR3 Script Aid ,上面有关于DDR3-1866的参数配置建议如下:

Tony Radice

Ladies and Gentlemen -

    Would you please publish how to adjust the script for newer DDR parts? For example: I want to select a DDR3L-1866 part and modify the tool to accept. I have the appropriate data, but the script does not accept.

 

Thank You.

    有用   喜欢  0回复
    • LinWang

      Hello Tony,

      Yes, There is no DDR3-1866 related parameters in aid.

       

      And after internal check and consult DDR vendor, we believe using DDR3-1600 parameters and run on DDR3-1866 grade chip is acceptable.

      No potential risk.

      That's why I did not update the aid.

       

      During discussion this topic, DDR vendor generally suggest to use DDR3-1066 parameters (which match real working speed).

      Hope above info can help you.

      @LinWang ,

             您好,DDR3-1866使用DDR3-1600的配置参数,或者是1066等的参数,都无法进行校准和压力测试呢?能否提供一下DDR3-1866的配置参数案例(针对IMX6Q的)。谢谢!

    0 项奖励
    回复

    4,389 次查看
    LinWang
    NXP Employee
    NXP Employee

    No special consideration on script when using DDR3-1866 chip.

    Please ask local FAE or DFAE for help to check HW first.

    0 项奖励
    回复

    4,389 次查看
    yz_z
    Contributor III

         您好,如果是配置参数的脚本参数不正确,怎么会不通过呢,感觉还是哪些相关寄存器配置上有问题。在硬件上应该是没有问题的吧,使用DDR3-1600都没有问题呢。

    0 项奖励
    回复

    4,389 次查看
    igorpadykov
    NXP Employee
    NXP Employee

    Hi yz

    DDR3-1866 chip may produce more noise (as it is faster) so one

    can try to decrease drive strength and pay attention to power supplies.

    Please check i.MX6 System Development User’s Guide considerations

    https://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

    Best regards
    igor

    0 项奖励
    回复