IMX6DQ firmware

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6DQ firmware

1,472件の閲覧回数
khaledali
Contributor III

I want to know if IMX6DQ series have the same firmware code which is  on the ROM chip ?
and
Is it an open source firmware that i can read and modify ?
and
If yes can anyone give me a link to read from ? !

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,324件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Khaled

ROM sources are not open source and can not be changed,

also sources are not available for customers, sorry.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

1,324件の閲覧回数
khaledali
Contributor III

Ok is there any way to put any other firmware on the ROM chip ?

0 件の賞賛
返信

1,324件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

no, as ROM is one time programmable memory.

~igor