IMX6DL Test gigabit ethernet fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DL Test gigabit ethernet fail

876 Views
frankweng
Contributor III

您好!

yoctol kernel 4.1.15 + ubuntu 16.04 & android6.0 m6.0.1_2.0.0-ga 都有一樣的問題

HW:IMX6DL+AR8031

使用iperf -s 在測試

1:giga lan ,測試結果不到5Mbits/sec

2:10/100 就能達到 90 Mbits/sec 左右

是否有任何的修正檔可以協助,謝謝

Labels (3)
0 Kudos
Reply
2 Replies

770 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frank

one can try NXP Demo Image

i.MX 6QuadPlus, i.MX 6Quad, i.MX 6DualPlus, i.MX 6Dual, i.MX 6DualLite, i.MX 6Solo Linux Binary Demo...

and check suggestions for rgmii on

i.MX6 Gigabit Ethernet - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

770 Views
frankweng
Contributor III

謝謝 igorpadykov 回應

Boundary Devices的方式試過,結果一樣

相同的ethernet code ,在其他專案的板子是OK
在7專案板子,惟一的專案ethernet giga的速度 test fail

此專案在去年年底才進行,HW上是跟其他專案一樣的線路

第一板HW 就發生 giga lan test fail

經過改板,將imx6dl 到ar8031 距離縮短,結果一樣test giga lan fail
是否除Boundary Devices的方式之外的解決方案,請求協助,謝謝

0 Kudos
Reply