IMX6DL - PC does not recognise the IMX6 cpu as USB OTG device

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DL - PC does not recognise the IMX6 cpu as USB OTG device

1,569 Views
georgiadede
Contributor I

We are using the IMX6U5DVM10ACR and the OTG USB port as device so the MFG tool can be used.

No software loaded and processor input/output supplies and clock look ok.  The connect a USB cable from my PC to the OTG USB port connector (before using the MFG tool). My PC does not recognize the IMX6 CPU as device (expect a new HID device in Win 'device manager'). I have attached the schematic for reference. Please can you take a look and assist? I suppose at that stage the Boot pins configuration settings are not relevant.

Also a couple of questions regarding the microprocessor output (LDOs) supplies.

According to the HW User guide Table 4-1 and Note 1 VDDSOC_CAP & VDDPU_CAP are allowed to be connected together. Is this right as this is the way I have implemented this on my design? I noticed that the SABRE design has these supplies on different rails.

 

Thank you.

Labels (2)
0 Kudos
Reply
2 Replies

1,447 Views
georgiadede
Contributor I

Clock is stable and has been checked. However, I have an issue with the POR_N signal (PMIC to IMX6 CPU reset) . The reset line is asserted and then goes high before (approx. 270us) the VDD_ARM_CAP and VDD_PU_CAP supplies become stable. This violates the power on sequence requirements.  Any suggestion to delay the POR_N signal? I can add a small supervisory device to delay the signal but let me know whether you see a quick solution to this.

Thank you.

0 Kudos
Reply

1,447 Views
igorpadykov
NXP Employee
NXP Employee

Hi georgiadede

reason may be 24MHz, please check if it is stable, use clock recommendations

given in i.MX6 System Development User’s Guide

http://www.nxp.com/docs/en/user-guide/IMX6DQ6SDLHDG.pdf

Recommended to follow SABRE design VDDSOC_CAP & VDDPU_CAP connections

as linux may turn off VDDPU_CAP in low power modes.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

 

0 Kudos
Reply