IMX6DL DI0_PIN15 andriod 5.0 device tree gpio config

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6DL DI0_PIN15 andriod 5.0 device tree gpio config

1,406 Views
linw
Contributor I

How can I config the DI0_PIN15 as LCD_ENABLE pin in the Device Tree

my config in DT as below: //but the pin can't be pull up in the driver yet!!!!!

mxcfb1: fb@0 {

compatible = "fsl,mxc_sdc_fb";

disp_dev = "ldb";

interface_pix_fmt = "RGB24";

mode_str ="1280x800@60";

default_bpp = <18>;
int_clk = <0>;
late_init = <0>;
pinctrl-names = "default";
pinctrl-0 = <&pinctrl_ipu1_1>;
my_lcd = <&gpio4 17 GPIO_ACTIVE_HIGH>;
status = "ok";
};


this code is what I do in the driver,but the pin can not be pull up
ret = devm_gpio_request_one(&pdev->dev, plat_data->gpio_int,
GPIOF_OUT_INIT_HIGH,
"my_lcd");
if (ret)
printk("---->error\n");

printk(" xxxx= ret = %d\n", ret);

lcd_enable = gpio_get_value(plat_data->gpio_int);
printk("init hi..shady---->get_lcd_eanble = %d\n", lcd_enable);

/* set high and read */
gpio_set_value(plat_data->gpio_int, 1); ///can not pull up!!!!!, don't know why???
lcd_enable = gpio_get_value(plat_data->gpio_int);

0 Kudos
Reply
1 Reply

1,151 Views
igorpadykov
NXP Employee
NXP Employee

Hi lin

DI0_PIN15 is special pin (can not be used as gpio) controlled by microcode in

file ipu_disp.c, refer to attached Linux Manual Table 6-1. IPU Driver Files and imx6qdl-sabresd.dtsi

how it can be used

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply