参考IMX6DUALLITE开发板画了一个板子,PMIC输出各路电压和时序都正确,上电后24MHZ晶振起振,32.768KHZ晶振空贴,连接电脑后显示无法识别的设备,但是在LINUX操作系统下可以显示HID信息,板子上USB_OTG_ID这个管脚我画在了GPIO_1,未做上下拉处理,开发板上USB_OTG_ID用的是ENET_RX_ER管脚,会不会是这个原因引起的或者还有其他原因。
HI,DAN WANG
USB_OTG_ID我用的是GPIO_1管脚,必须使用ENET_RX_ER管脚吗?板上ENET_RX_ER管脚是悬空的末引出来。用GPIO_1行不行?谢谢。
Hi yin kai,
It's OK that you use the GPIO_1 for USB_OTG_ID. But the voltage should be provided right.
Here you can refer to iMX6DL : Is the USB_OTG_ID pin necessary for USB boot (Serial Downloader) ? . Hope this can help you.
Have a nice day
Dan
Hi yin kai,
Here it caused by the USB_OTG_ID, the USB_OTG_ID pin need 2.5 V or 3.3 V voltage. Details you can refer to the IMX6DL
datasheet and you also can refer to our reference board design.
On the USB_OTG no Recognized, you can do the follows test:
1\BOOT_MODE0 = 1; BOOT_MODE1 = 0
2\USB_OTG_ID pin 2.5 V or 3.3 V voltage
3\ The USB_OTG_VBUS of CPU need 5 V voltage
Have a great day,
Dan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Mark Correct button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
USB_OTG_ID这个管脚我画在了GPIO_1上了,必须要用ENET_RX_ER管脚吧,现在ENET_RX_ER管脚是悬空的。谢谢