IMX6D - HDMI to VGA conversion

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6D - HDMI to VGA conversion

881 Views
ashasampathkuma
Contributor I

Hi all ,

we are working on a custom board based of imx6d and using Android M 6.0.1_1.0.1 BSP version.

Our board has an 7 inch display and uses LVDS interface.The LVDS display is working. We need to mirror the LVDS display contents to a VGA monitor.The screen mirroring is working for HDMI monitor but not for VGA.

We connected our board to  VGA monitor using HDMI to VGA adapter cable. The HDMI driver is unable to read the EDID data from monitor.

Whether imx hdmi driver supports VGA monitor?

Thanks,

Asha

Labels (4)
0 Kudos
Reply
1 Reply

677 Views
igorpadykov
NXP Employee
NXP Employee

Hi Asha

I am afraid imx hdmi driver does not support VGA monitor.

Only "true" HDMI monitor can send EDID information.

May be useful to look at similar description with DVI

DVI Support on i.MX6 boards - Boundary Devices 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply