IMX6 solo MMDC running at up to 396 MHz, Our DDR3L chip is 800MHz.
Queries:
1. How the DDR3L chip frequency down converted to 396MHz and interact with IMX6 solo MMDC controller?
2. Shall we change the frequency of DDR3L through Software? if this is yes please provide me the Details which will help us.
Thanks & Regards,
Rameshkumar
Hello,
It is needed to configure the DDR3 device for 400 MHz.
Please use the following resource how to implement DDR initialization.
DRAM Customization on i.MX6x | NXP Community
As for 0S (Linux) level, please refer to Chapter 1 (Porting U-Boot from an i.MX 6/7
Reference Board to an i.MX 6/7 Custom Board) of “i.MX_BSP_Porting_Guide.pdf”
in Linux documentation.
http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Can we change DVFS in kernel can we change the DDR frequecy as per product needs?