IMX6 security reference manual

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 security reference manual

3,155 次查看
jacques
Contributor I

Hello,

I have the imx6 security reference manual, but it only covers the chips Dual, Qual, Solo and DualLite.

Where can I get information about the security features of other chips in the imx6 family?

According to this:

http://cache.freescale.com/files/32bit/doc/brochure/FLYRIMXPRDCMPR.pdf

for instance the imx6 UltraLite has some different security functionalities.

Thank you,

Jacques

0 项奖励
回复
1 回复

1,470 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Jacques

these documents can be obtained from local FAE,

note one needs to have NDA

1.jpg

i.MX 6UltraLite Applications Processor|Freescale

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复