I need to add some 2.5 V GPIO pins to my IMX6 DualLite design, and for various reasons the only place I can put them is on EIM1 and 2. I need to leave EIM0 at 3.3 V. So I'd be powering EIM0 from 3.3 V and EIMs 1 and 2 from 2.5 V.
As far as I can tell this shouldn't be an issue for GPIO eFuse override at boot. Does anyone know whether this could be an issue?
Yes, I could just use a level translator, but...I can't.
Thanks,
Nick
Hi Nick
no, there will no issues with powering EIM0 from 3.3 V and EIMs 1 and 2 from 2.5 V,
does not matter GPIO eFuse override at boot
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------