IMX6 dual cam0 or cam1 port de-multiplexing DVP camera stream

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX6 dual cam0 or cam1 port de-multiplexing DVP camera stream

590 次查看
Yogee
Contributor III

Hi,

we would like to know if CAM0 or CAM1 supports 8 bit DVP data from video decoder with 4 camera streams.

标签 (2)
0 项奖励
回复
1 回复

489 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Yogee

yes one can connect 4 cameras using MIPI CSI-2, for that it is necessary to

multiplex the four streams in an FPGA. Each camera in this case

should use a different stream identifier (stream 0-3).

Those 4 data streams can the be distributed across the 4 CSI (per IPU

there are two CSI modules available in the i.MX6DQ).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复