IMX6 dual cam0 or cam1 port de-multiplexing DVP camera stream

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 dual cam0 or cam1 port de-multiplexing DVP camera stream

459 Views
Yogee
Contributor III

Hi,

we would like to know if CAM0 or CAM1 supports 8 bit DVP data from video decoder with 4 camera streams.

Labels (2)
0 Kudos
1 Reply

358 Views
igorpadykov
NXP Employee
NXP Employee

Hi Yogee

yes one can connect 4 cameras using MIPI CSI-2, for that it is necessary to

multiplex the four streams in an FPGA. Each camera in this case

should use a different stream identifier (stream 0-3).

Those 4 data streams can the be distributed across the 4 CSI (per IPU

there are two CSI modules available in the i.MX6DQ).

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos