IMX6 and QT 5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 and QT 5

1,069 Views
conti_rob
Contributor II

Hello, i hope someone here can help me. I have a Problem by the installation from QT.

Thanks

Warning: Disabling pkg-config since PKG_CONFIG_LIBDIR is not set.
Note: PKG_CONFIG_SYSROOT_DIR automatically set to /home/udcu/LTIB/litb/rootfs
The OpenGL ES 2.0 functionality test failed! You might need to modify the include and library search paths by editing QMAKE_INCDIR_OPENGL_ES2, QMAKE_LIBDIR_OPENGL_ES2 and QMAKE_LIBS_OPENGL_ES2 in /home/udcu/qt5/qtbase/mkspecs/devices/linux-imx6-g++.

Labels (3)
3 Replies

508 Views
YixingKong
Senior Contributor IV

Barth

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos

508 Views
YixingKong
Senior Contributor IV

Barth

Had your issue got resolved? If yes, we are going to close the discussion in 3 days. If you still need help, please feel

free to reply with an update to this discussion.

Thanks,
Yixing

0 Kudos

507 Views
VladanJovanovic
NXP Employee
NXP Employee

There's a small test program that is compiled during configure stage to test for OpenGL library presence. You may try to compile it manually and see why it fails to compile. Usually it is missing library for the GPU, as there's a few of them needed to be included.