Hello,
I'm not an expert, so thank you for being patient with me.
I am working on using gstreamer on an IMX6 quad core processor to output some video with an image overlay. (3.0.35 Kernel, Yocto OpenEmbedded)
It is working great, except that I would like to change how much transparency exists.
I keep seeing a variable in other posts, VSALPHA=1 . Can anyone shed some light, or point me to some documentation, as to how this is used with Gstreamer?
Here are my gstreamer lines:
gst-launch tvsrc device=/dev/video0 ! mfw_v4lsink disp-width=1279 disp-height=720 device=/dev/video17 &
gst-launch filesrc location=/home/root/tlogo.png ! pngdec ! imagefreeze ! ffmpegcolorspace ! fbdevsink device=/dev/fb0 &
Thank you,
Ryan
已解决! 转到解答。
struct mxcfb_gbl_alpha g_alpha;
g_alpha.alpha = 127; //alpha value
g_alpha.enable = 1;
if ((fd_fb_0 = open("/dev/fb0", O_RDWR )) < 0) {
printf("Unable to open frame buffer 0\n");
return TFAIL;
}
if (ioctl(fd_fb_0, MXCFB_SET_GBL_ALPHA, &g_alpha) < 0) {
printf("Set global alpha failed\n");
close(fd_fb_0);
return TFAIL;
}
The source code above set a global value for alpha. Global means the whole screem.
Please, let me know if this is enough.
Hello Daiane,
Thank you for that information. I have been able to gather that information through other several discussion topics.
I was hoping to find something that was already integrated into Gstreamer and not be required to compiled the custom source code.
Given that the text 'VSALPHA=1' seems to be placed before some gstreamer pipelines on this site, I was curious if there was more integration and what this variable was achieving through which method.
Thanks,
Ryan