IMX6 UL PIN MULTIPLEXING

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 UL PIN MULTIPLEXING

892件の閲覧回数
Hamza_Hassan
Contributor I

Hi

I am using IMX6.UL processor pin . I am using RS232 transmitter using serial port. Can i use the same pin as GPIO for transmitting IR signal.

Is there any support in IMX6?

Please guide me on this.

 

Thanks

0 件の賞賛
返信
3 返答(返信)

873件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Hamza_Hassan,

Hope you are doing well.

One can check the Available mux options of the pin which is configured as a RS232 Transmitter in RM. If the possible pad is GPIO*, then you can configure the same pin as a GPIO for transmitting IR signal.
Please note that once you configure this pin as a GPIO, After that you will not be able to use the same pin as Rs232 Transmitter.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信

846件の閲覧回数
Hamza_Hassan
Contributor I

Hi @riteshmpatel ,

Hope you are doing well.

Can I configure the pin at runtime?

Or should I need to reboot every time for new configuration?

Thanks

Hamza Hassan

0 件の賞賛
返信

837件の閲覧回数
riteshmpatel
NXP TechSupport
NXP TechSupport

Hi @Hamza_Hassan,

Unforutnately, doing runtime configurations is not possible.

The configurations must be done in dts.

Thanks & Regards,
Ritesh M Patel

0 件の賞賛
返信