IMX6 SoloX: Unable to boot from QSPI NOR FLASH

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 SoloX: Unable to boot from QSPI NOR FLASH

6,917件の閲覧回数
joilg
Contributor I

Hello,

I  am working on a customized IMX6 Solo X Board with a  Spansion FL128S Serial NOR Flash  attached on the QSPI2  Interface.

U-Boot works well when booting with imx-usb-loader over USB and I am able to read and write the NOR Flash within u-Boot.

Then I setup Flash and Boot options to boot from QSPI, but the device is not booting.

Flash Content is:

->  sf probe; sf read 80800000 0 60000

SPI Conf. Parametr    at 0x400:

80800400: 00000000 00000000 00000000 00000000    ................

80800410: 00000000 00000000 01000000 02000000    ................

80800420: 00000000 00000000 00000000 04000000    ................

80800430: 00000000 00000000 00000001 00000000    ................

80800440: 00000001 00000000 00000000 00000000    ................

80800450: 00000000 00000000 00000000 00000000    ................

80800460: 00000000 00000000 0818040b 1c080c08    ................

80800470: 00002400 00000000 00000000 00000000    .$..............

80800480: 00000000 00000000 00000000 00000000    ................

80800490: 00000000 00000000 00000000 00000000    ................

808004a0: 00000000 00000000 00000000 00000000    ................

808004b0: 00000000 00000000 00000000 00000000    ................

808004c0: 00000000 00000000 00000000 00000000    ................

808004d0: 00000000 00000000 00000000 00000000    ................

808004e0: 00000000 00000000 00000000 00000000    ................

808004f0: 00000000 00000000 00000000 00000000    ................

80800500: 00000000 00000000 00000000 00000000    ................

80800510: 00000000 00000000 00000000 00000000    ................

80800520: 00000000 00000000 00000000 00000000    ................

80800530: 00000000 00000000 00000000 00000000    ................

80800540: 00000000 00000000 00000000 00000000    ................

80800550: 00000000 00000000 00000000 00000000    ................

80800560: 00000000 00000000 03000000 00000000    ................

80800570: 00000000 00000000 00000000 00000000    ................

80800580: 00000000 00000000 00000000 00000000    ................

IVT Table at 0x1000:

80801000: 402000d1 87800000 00000000 877ff42c    .. @........,...

80801010: 877ff420 877ff400 00000000 00000000     ...............

DCD  at 0x102c:

8080102c: 400802d2                               ...@

80801030: 040402cc 68400c02 ffffffff 6c400c02    ......@h......@l

80801040: ffffffff 70400c02 ffffffff 74400c02    ......@p......@t

80801050: ffffffff 78400c02 ffffffff 7c400c02    ......@x......@|

80801060: ffffffff 80400c02 ffffffff 84400c02    ......@.......@.

80801070: ffffffff 18060e02 00000c00 fc050e02    ................

80801080: 00000000 2c030e02 30000000 00030e02    .......,...0....

80801090: 20000000 fc020e02 20000000 f4050e02    ... ....... ....

808010a0: 20000000 40030e02 20000000 20030e02    ... ...@... ...

808010b0: 00000000 10030e02 20000000 14030e02    ........... ....

808010c0: 20000000 14060e02 20000000 f8050e02    ... ....... ....

808010d0: 00000200 30030e02 28000000 34030e02    .......0...(...4

808010e0: 28000000 38030e02 00000000 3c030e02    ...(...8.......<

808010f0: 00000000 08060e02 00000200 0c060e02    ................

80801100: 28000000 10060e02 28000000 1c060e02    ...(.......(....

80801110: 00000000 20060e02 00000000 ec020e02    ....... ........

80801120: 28000000 f0020e02 28000000 f4020e02    ...(.......(....

BDS at 0x1020:

80801020: 87800000 00200000 00000000             ...... .....

u-Boot at 0x01c00:

80801c00: ea0000be e59ff014 e59ff014 e59ff014    ................

80801c10: e59ff014 e59ff014 e59ff014 e59ff014    ................

80801c20: 87800060 878000c0 87800120 87800180    `....... .......

80801c30: 878001e0 87800240 878002a0 deadbeef    ....@...........

SPI Port Mux is

MX6_PAD_NAND_WP_B__QSPI2_A_DATA_0

MX6_PAD_NAND_READY_B__QSPI2_A_DATA_1

MX6_PAD_NAND_CE0_B__QSPI2_A_DATA_2

MX6_PAD_NAND_CE1_B__QSPI2_A_DATA_3

MX6_PAD_NAND_ALE__QSPI2_A_SS0_B

MX6_PAD_NAND_CLE__QSPI2_A_SCLK

MX6_PAD_NAND_DATA07__QSPI2_A_DQS

Boot Pins:  (Boot from QSPI2)

LCD1_DATA03 High

LCD1_DATA04 High

LCD1_DATA05 Low

LCD1_DATA06 Low

LCD1_DATA07 Low

I measured a activity on SPI Pins for 240us for reading 8 Blocks of 64 Bytes bofor switching to usb activating.

Can someone take a lock on the Flash Content.  Also a working Flash Image of a similar IMX6SX Board would be helpful.

Best Regards

Johannes

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,115件の閲覧回数
joilg
Contributor I

Hello,

finally got it booting.

Booting U-Boot from QSPI-NOR Flash requires an other offset in Flash as booting from NAND Flash.  

NAND-Flash:   Uboot image at 0x400

SPI-NOR:        QSPI-Configuration Parameter at 0x0400

                      Uboot image at 0x400                        

Due to the other offset I have to adjust the Boot Table:

My U-Boot-Image begins with:

pastedImage_6.png 

The Boot Table  Structure is at 0x20

U-Boot Relocation Address at  0x20: 877FF000

            relocation length at      0x24: 00050000

I add 0xc00 to the 4-byte value at 0x20    -> 0x877FE400: 

and correct the length with the size of uboot image + 0xc00 

following script did it for me:

mw.b 80800000  00 60000

sf probe

sf erase 0 60000

dhcp  80800400 qspic.imx

dhcp  80801000 uboot.imx

mw  80801020 877FE400

mw  80801024 00050C00

sf write  80800000 0 60000

qspic.imx is the image of the QSPI Configuration Table (512Bytes)

I use a board specific paches for Uboot Version 2015.01.

  

Regards

Johannes

0 件の賞賛
返信

3,115件の閲覧回数
alejandrolozan1
NXP Employee
NXP Employee

Hi,

Can you share the QuadSPI Configuration Parameters? I assume that you generated from an existing structure in C code or it was appended to the binary file in certain way.

That would help to understand the possible wrong QuadSPI configuration.

Regards,

Alejandro

0 件の賞賛
返信

3,115件の閲覧回数
joilg
Contributor I

Hi Alejandro,

with help from Freescale, I am able now to read successful the SPI Configuration Parameter from Flash in 240us, then I notice now reading from flash for the 358us. No Message at the console.

I assume either Device Configuration or U-Boot are not correct configured. 

I use U-Boot Version 2015.01 with a board specific patch.

For Flashing i use following script within U-boot:

setenv uimg 'boot/uboot.imx'

# clear memory,flash

setenv uclr 'mw.b  ${loadaddr}  00 0x180000; sf probe; sf erase 0 180000'

# SPI Parameter  0x400..0x800

setenv uspi 'mw 8080041C 02000000; mw 80800420 3; mw 80800424 3; mw 80800428 08000000; mw 80800430 08000000; mw 80800440 1;  mw 80800568 01000001;  mw 808005fc C0FFEE01'

# Look up table

setenv ulps 'echo "lutps"; mw  80800468 0818040B; mw  8080046C 1C040C08; mw  80800470 00002400'

# Correct Decice Configuration 0x102c

setenv udcd 'mw  8080102C 410401d2;  mw 808010e8 28000000; mw 808010F0 28000000; mw 80801108 28000000; mw 80801110 28000000; mw 80801130 28000000; mw 80801138 28000000; mw 80801168 42404040; mw 80801170 383C4040; mw 808011F0 00001882'

setenv uflash 'run uclr; dhcp  80801000 ${uimg}; run uspi; run ulps; run udcd; sf probe;  sf write ${loadaddr} 0000  180000'

save

run uflash

Best Regards

Johannes

0 件の賞賛
返信