IMX6 Solo not able to boot from EMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Solo not able to boot from EMMC

761 Views
mahmood_md
Contributor I

imx6solo‌ uboot‌  emmc  boot‌

I am working on a custom imx6 solo board.

I am trying to write u-boot on the very first time to emmc, and able to write through DFU and UMS tool.

after successful written when I power off and change to boot mode(jumper)., I do not get any print or logs on the serial console.

with the same image, I am able to load on RAM itself and boot successfully.

Can you please help me to resolve this issue ASAP.

Your help is highly appreciated

Thanks,

Isharat

Labels (5)
0 Kudos
Reply
1 Reply

682 Views
igorpadykov
NXP Employee
NXP Employee

Hi Isharat

issue may be related to signal integrity as described on

eMMC 8GB to 4GB - crash on linux (yocto) boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply