IMX6-Q stucks at "stopping system v runlevel compatibility"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6-Q stucks at "stopping system v runlevel compatibility"

933 Views
rajathks
Contributor II

Not able to boot IMX6-Q as it get stucked at "stopping system v runlevel compatibility" . Please provide me a solution

Here is the link that i have followed to configure the IMX6-Q

Installing Ubuntu Rootfs on NXP i.MX6 boards 

Screenshot_of_console.png

Labels (2)
0 Kudos
2 Replies

541 Views
b36401
NXP Employee
NXP Employee

Most likely there is something wrong with window manager.
Please check .xsession-errors file for the user is used for autologin.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

541 Views
rajathks
Contributor II

Thank you for the reply ...Where im suppose to check ? In target or Host ?

Regards,

Raj

0 Kudos