IMX6 - Problems with gstreamer mfw_v4lsrc (on Boundary Devices Sabre-Lite)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 - Problems with gstreamer mfw_v4lsrc (on Boundary Devices Sabre-Lite)

1,628 Views
TomMorrison
Contributor III

Hi,

I am wondering if anybody else is having issues with the gstreamer (gst-fsl-plugin) mfw_v4lsrc.

I am using LTIB 12-09 version (downloaded from Extranet) - as follows:

-----

root@Tom ~$ gst-inspect mfw_v4lsrc

MFW_GST_V4LSRC_PLUGIN 3.0.1 build on Nov  1 2012 14:31:47.

Factory Details:

  Long name:    v4l2 based camera src

  Class:        Src/Video

  Description:  Capture videos by using csi camera

  Author(s):    Multimedia Team <shmmmw@freescale.com>

  Rank:         primary (256)

Plugin Details:

  Name:                 v4lsrc.imx

  Description:          v4l2-based csi camera video src

  Filename:             /usr/lib/gstreamer-0.10/libmfw_gst_v4lsrc.so

  Version:              3.0.1

  License:              LGPL

  Source module:        gst-fsl-plugins

  Binary package:       Freescle Gstreamer Multimedia Plugins

  Origin URL:           http://www.freescale.com

GObject

+----GstObject

       +----GstElement

             +----GstBaseSrc

                   +----GstPushSrc

                         +----MFWGstV4LSrc

Pad Templates:

  SRC template: 'src'

    Availability: Always

    Capabilities:

      ANY

Element Flags:

  no flags set

Element Implementation:

  Has change_state() function: gst_base_src_change_state

  Has custom save_thyself() function: gst_element_save_thyself

  Has custom restore_thyself() function: gst_element_restore_thyself

Element has no clocking capabilities.

Element has no indexing capabilities.

Element has no URI handling capabilities.

Pads:

  SRC: 'src'

    Implementation:

      Has getrangefunc(): gst_base_src_pad_get_range

      Has custom eventfunc(): gst_base_src_event_handler

      Has custom queryfunc(): gst_base_src_query

      Has custom iterintlinkfunc(): gst_pad_iterate_internal_links_default

      Has getcapsfunc(): gst_base_src_getcaps

      Has setcapsfunc(): gst_base_src_setcaps

      Has acceptcapsfunc(): gst_pad_acceptcaps_default

Aborted

----


If I use Timesys version (using web based linuxlink) this works just fine!


I am not sure what is going on here?


Tom

Labels (1)
0 Kudos
4 Replies

726 Views
YixingKong
Senior Contributor IV

TOm

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos

726 Views
YixingKong
Senior Contributor IV

TOm

We have not got your response yet and will close the diacussion in 3 days. If you still need help, please feel free to

reply with an update to this discussion.
Thanks,
Yixing

0 Kudos

726 Views
YixingKong
Senior Contributor IV

Tom

We are sorry for getting back to you so late. Are you still stuck with the issue? If you have somehow to resolved the issue, can we close the discussion? If you still need Freescale help, please feel free to contact us.

Thanks,

Yixing

0 Kudos

726 Views
daiane_angolini
NXP Employee
NXP Employee

this is the only problem you faced?

I've never payed attention if this happened to my anytime.

0 Kudos