IMX6 MMDC fast or slow precharge PD?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 MMDC fast or slow precharge PD?

Jump to solution
755 Views
timharvey
Contributor IV

The spreadsheet/script in https://community.freescale.com/docs/DOC-94917 sets MDPDC bit7 SLOW_PD=0 indicating fast precharge PD mode, yet the MR0 value written to the DRAM sets bit12=0 indicating slow precharge PD. The TRM states in the description of MDPDC SLOW_PD that it should be set the same as memory (which makes sense). Therefore I believe the spreadsheet/script to be in error.


Does Freescale have any recommendations on if the values should be set to fast precharge PD or slow?

Regards,

Tim

arpan_chakravarty

Kevin Wong

LinWang

gateworks

proven_partner

Labels (6)
Tags (1)
0 Kudos
1 Solution
495 Views
LinWang
NXP Employee
NXP Employee

Sorry for pending a long time.

The configuration should be aligned on both controllor and DDR device side.

Fast or slow mode should depend on real application, that's a trage off between power consumption and working efficiency.

Thanks for digging it out!

View solution in original post

0 Kudos
2 Replies
496 Views
LinWang
NXP Employee
NXP Employee

Sorry for pending a long time.

The configuration should be aligned on both controllor and DDR device side.

Fast or slow mode should depend on real application, that's a trage off between power consumption and working efficiency.

Thanks for digging it out!

0 Kudos
495 Views
LinWang
NXP Employee
NXP Employee

Had Involved design team.

Due to NPI urgent schedule, will check this question next week.

Suppose getting update before end of next week.

0 Kudos