IMX6 - IPU CSI IC MEM path with output greater than 1024

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 - IPU CSI IC MEM path with output greater than 1024

807 Views
allan-navarro
Contributor I

Hello 

I'm using the CSI IC MEM path to scale the images coming directly from the CSI without going to memory first. I know the limitation of 1024 pixels and I know it's possible to split the buffer into two stripes to handle greater sizes. I'm wondering if it is possible to make this split when image comes from the CSI and not from memory?

I'm using the ioctl VIDIOC_S_INPUT to choose the path and also setting  fmt.fmt.pix to the desired scaled output. I'm curious how can I specify this task split?

Embedded SW Engineer at RidgeRun

Contact us: support@ridgerun.com
Developers wiki: https://developer.ridgerun.com/
Website: www.ridgerun.com
Tags (2)
0 Kudos
Reply
1 Reply

781 Views
Bio_TICFSL
NXP TechSupport
NXP TechSupport

Hello,

As far as I know this is a limitation of IPU, but it sounds possible what you asked but when the IPU appears it won't work.

regards

0 Kudos
Reply