IMX6 ESAI TDM mode configuration in driver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX6 ESAI TDM mode configuration in driver

跳至解决方案
3,020 次查看
dp_yanam
Contributor I

Hi everyone,

i was new to IMX6 yocto. we trying to interface ADC chip in frame sync (ADS1274)  using  ESAI TDM mode.

Can anyone please tell me what is easiest way to implement driver & application to use for it.

Please share if you have any information related to ESAI configurations for above chip in device tree.

Thanks in advance,

K.durgaprasad

标签 (2)
0 项奖励
回复
1 解答
2,734 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Durgaprasad

one can look at audio drivers described in

Linux L4.14.78_1.0.0 Documentation

and use them as starting point.

Best regards
igor

在原帖中查看解决方案

0 项奖励
回复
5 回复数
2,734 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Durgaprasad

tdm is supported in esai driver using fsl_esai_set_dai_tdm_slot() function

linux/sound/soc/fsl/fsl_esai.c

fsl_esai.c\fsl\soc\sound - linux-imx - i.MX Linux kernel 

in fsl_esai_startup() : /* Set a default slot number -- 2 */

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
2,734 次查看
dp_yanam
Contributor I

Hi igor,

 

Thanks for your reply. i had gone through "fsl_esai.c" file. I want to know like we need to write a new driver for ADS1274 to get frame sync TDM mode on ESAI or SSI interface. Can you please tell me the procedure to get the communication up. we want to interface ADC without codec to imx6 process for capture the data from ADC.

 

Thanks & Regards,

K.durgaprasad.

0 项奖励
回复
2,735 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Durgaprasad

one can look at audio drivers described in

Linux L4.14.78_1.0.0 Documentation

and use them as starting point.

Best regards
igor

0 项奖励
回复
2,734 次查看
dp_yanam
Contributor I

Hello igor,

         i could able to work on SSI TDM mode configurations. my driver is working fine with interfacing the  SSI with ADC.

We want to generate 24MHz master clock (SCLK) & FS clock 48KHz. Can you please tell me the configurations for the clock. i was try to change the master clock settings in driver but it was generating only 2.45MHz.

Thanks & regards,

K. durgaprasad

0 项奖励
回复
2,734 次查看
dp_yanam
Contributor I

Hello igor,

Thanks for sharing the documents. I  will start from scratch & let you know if i facing any issues.

Thanks & regards,

K. durgaprasad.

0 项奖励
回复