IMX6 ESAI TDM mode configuration in driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 ESAI TDM mode configuration in driver

ソリューションへジャンプ
2,985件の閲覧回数
dp_yanam
Contributor I

Hi everyone,

i was new to IMX6 yocto. we trying to interface ADC chip in frame sync (ADS1274)  using  ESAI TDM mode.

Can anyone please tell me what is easiest way to implement driver & application to use for it.

Please share if you have any information related to ESAI configurations for above chip in device tree.

Thanks in advance,

K.durgaprasad

ラベル(2)
0 件の賞賛
返信
1 解決策
2,699件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Durgaprasad

one can look at audio drivers described in

Linux L4.14.78_1.0.0 Documentation

and use them as starting point.

Best regards
igor

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
2,699件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Durgaprasad

tdm is supported in esai driver using fsl_esai_set_dai_tdm_slot() function

linux/sound/soc/fsl/fsl_esai.c

fsl_esai.c\fsl\soc\sound - linux-imx - i.MX Linux kernel 

in fsl_esai_startup() : /* Set a default slot number -- 2 */

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,699件の閲覧回数
dp_yanam
Contributor I

Hi igor,

 

Thanks for your reply. i had gone through "fsl_esai.c" file. I want to know like we need to write a new driver for ADS1274 to get frame sync TDM mode on ESAI or SSI interface. Can you please tell me the procedure to get the communication up. we want to interface ADC without codec to imx6 process for capture the data from ADC.

 

Thanks & Regards,

K.durgaprasad.

0 件の賞賛
返信
2,700件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Durgaprasad

one can look at audio drivers described in

Linux L4.14.78_1.0.0 Documentation

and use them as starting point.

Best regards
igor

0 件の賞賛
返信
2,699件の閲覧回数
dp_yanam
Contributor I

Hello igor,

         i could able to work on SSI TDM mode configurations. my driver is working fine with interfacing the  SSI with ADC.

We want to generate 24MHz master clock (SCLK) & FS clock 48KHz. Can you please tell me the configurations for the clock. i was try to change the master clock settings in driver but it was generating only 2.45MHz.

Thanks & regards,

K. durgaprasad

0 件の賞賛
返信
2,699件の閲覧回数
dp_yanam
Contributor I

Hello igor,

Thanks for sharing the documents. I  will start from scratch & let you know if i facing any issues.

Thanks & regards,

K. durgaprasad.

0 件の賞賛
返信