IMX6 EIM chip select address range partitioning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 EIM chip select address range partitioning

1,074 Views
brianbusingye
Contributor I

Hi,

Please clarify the following.

1) I would like to partition the EIM chip selects to 32M, is this done by setting IOMUXC_GPR1[1:2] = IOMUXC_GPR1[4:5] = IOMUXC_GPR1[7:8] = IOMUXC_GPR1[10:11] = 0

2) As specified on page 1955 of IMX6DQ Applications Processor Manual, if the address range of the four chip selects is set to 32M is the range below for each chip select correct

CS0: 0x8000000 -> 0x9FFFFFF

CS1: 0xA000000 -> 0xBFFFFFF

CS2: 0xC000000 -> 0xDFFFFFF

CS3: 0xE000000 -> 0xFFFFFFF

Thanks

Brian

Labels (1)
0 Kudos
Reply
1 Reply

897 Views
igorpadykov
NXP Employee
NXP Employee

Hi Brian

I think your understanding is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply