IMX6 EIM chip select address range partitioning

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 EIM chip select address range partitioning

991件の閲覧回数
brianbusingye
Contributor I

Hi,

Please clarify the following.

1) I would like to partition the EIM chip selects to 32M, is this done by setting IOMUXC_GPR1[1:2] = IOMUXC_GPR1[4:5] = IOMUXC_GPR1[7:8] = IOMUXC_GPR1[10:11] = 0

2) As specified on page 1955 of IMX6DQ Applications Processor Manual, if the address range of the four chip selects is set to 32M is the range below for each chip select correct

CS0: 0x8000000 -> 0x9FFFFFF

CS1: 0xA000000 -> 0xBFFFFFF

CS2: 0xC000000 -> 0xDFFFFFF

CS3: 0xE000000 -> 0xFFFFFFF

Thanks

Brian

ラベル(1)
0 件の賞賛
返信
1 返信

814件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Brian

I think your understanding is correct.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信