IMX6 DDR Frequency change with newer u-boot

cancel
Showing results for 
Search instead for 
Did you mean: 

IMX6 DDR Frequency change with newer u-boot

160 Views
dennis3
Contributor IV

I built a custom image from the latest sources for the imx6q-sabresd board.  The image works fine but I'd like to change the u-boot to initialize the dram to a slower speed so we can test if our software will continue to perform properly.  There are a number of posts with this same question but the version of u-boot seems to be quite a bit different.  I'm using 2018.17.  The older posts refer to flash_header.S or a various DTC table versions which don't seem to have changed in the latest version.  Either that or I just don't know where to look which could also be the case.

Anyhow, anyone have a quick pointer to the right sources to start looking at?

Labels (3)
Tags (3)
0 Kudos
1 Reply

52 Views
igorpadykov
NXP TechSupport
NXP TechSupport

Hi Dennis

2018.17 version is not supported by nxp, it may be posted on uboot mail list.

U-Boot Info Page 

Latest nxp official uboot version is v2017.03_4.9.88, I am afraid it does not support

changing ddr frequency

uboot-imx - i.MX U-Boot 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos