Hi ,
MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment
Failed (-5)
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: vga
Err: vga
Currently we have received this log Can tell me what is the default environment for nxp mx6quad processor and How to change the Out and Err Port as serial?
Solved! Go to Solution.
@laulavanya
Hello,
according to section "Common kernel boot parameters" in "i.MX_Linux_Release_Notes.pdf":
when primary displaying on the CLAA-WVGA dumb parallel LCD panel.
video=mxcfb0:dev=lcd,CLAA-WVGA,if=RGB656
Regards,
Yuri.
Hi Yuri,
Why OUT and ERR is taking as "VGA" instead of serial . where I need to enable the serial for both OUT and ERR?
Hi yuri,
Linux version 4.14
Regards,
Lavanya
@laulavanya
Hello,
according to section "Common kernel boot parameters" in "i.MX_Linux_Release_Notes.pdf":
when primary displaying on the CLAA-WVGA dumb parallel LCD panel.
video=mxcfb0:dev=lcd,CLAA-WVGA,if=RGB656
Regards,
Yuri.