IMX6 Custom Board : Choosing Default Environment with VGA as out port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6 Custom Board : Choosing Default Environment with VGA as out port

Jump to solution
1,262 Views
laulavanya
Contributor II

Hi ,

MMC: FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... *** Warning - bad CRC, using default environment

Failed (-5)
No panel detected: default to Hannstar-XGA
Display: Hannstar-XGA (1024x768)
In: serial
Out: vga
Err: vga

Currently we have received this log Can tell me what is the default environment for nxp mx6quad processor and How to change the Out and Err Port as serial?

 

Labels (1)
0 Kudos
1 Solution
1,229 Views
Yuri
NXP Employee
NXP Employee

@laulavanya 
Hello,

  according to section "Common kernel boot parameters" in "i.MX_Linux_Release_Notes.pdf":

when primary displaying on the CLAA-WVGA dumb parallel LCD panel.

video=mxcfb0:dev=lcd,CLAA-WVGA,if=RGB656

Regards,
Yuri.

View solution in original post

5 Replies
1,217 Views
laulavanya
Contributor II

Hi Yuri,

Why OUT and ERR is taking as "VGA" instead of serial . where I need to enable the serial for both OUT and ERR? 

0 Kudos
1,249 Views
Yuri
NXP Employee
NXP Employee

@laulavanya 
Hello,

  what NXP Linux release is used in the case?

Regards,
Yuri.

0 Kudos
1,235 Views
laulavanya
Contributor II

Hi yuri,

Linux version 4.14

Regards,
Lavanya

0 Kudos
1,236 Views
laulavanya
Contributor II

Hi @Yuri ,

Currently using 4.14

 

Regards,
Lavanya

0 Kudos
1,230 Views
Yuri
NXP Employee
NXP Employee

@laulavanya 
Hello,

  according to section "Common kernel boot parameters" in "i.MX_Linux_Release_Notes.pdf":

when primary displaying on the CLAA-WVGA dumb parallel LCD panel.

video=mxcfb0:dev=lcd,CLAA-WVGA,if=RGB656

Regards,
Yuri.