IMX6 Android / Yocto DCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX6 Android / Yocto DCD

684件の閲覧回数
leonardoprates
Contributor III

Inside u-boot/board/freescale/mx6sabresd are there some DCD configs.

There are files with each register value using spaces, like below in mx6q_4x_mt41j128.cfg:

DATA 4 0x020e0798 0x000C0000

But in file mx6solo_4x_mt41j128.cfg  use a comma separated aproach

DATA 4, 0x020e0774, 0x000C0000

The DCD config parser accepts both or which one is correct for IMX6Q?

Thanks,

Leonardo

Ta

ラベル(5)
0 件の賞賛
返信
0 返答(返信)