IMX6的SSI的lrclk 问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6的SSI的lrclk 问题

763 Views
2570624484
Contributor II

Dear NXP :调试IMX6 的SSI,现在遇到一个问题,在播放1KHZ的正弦波的时候,总是有杂音。

软件在HAL层把数据dump出来,数据没有异常,硬件还把IIS输出来的数据记录下来,做成表格,还原数据,波形也没有异常。

怀疑点:测量lrclk的频率无法稳定在44.1K,大约在43.6xxKHz,这个是否可以优化,让SSI的lrclk稳定在44.1K,硬件实际是做了交叉实验的,把其他家的型号的SOC输出的1KHZ接到我们的DSP上,没有杂音,差异在lrclk上,因此硬件怀疑这个时钟导致DSP的数模转换异常。

IMX6 SSI--------DSP有杂音

其他SOC的IIS信号飞线到-----》DSP没有杂音

期待你的回复,感谢!

Labels (1)
0 Kudos
1 Reply

615 Views
igorpadykov
NXP Employee
NXP Employee

pastedImage_2.jpg

----------------------------------

 Irc6 SSI lrclk problem
Dear NXP: Debugging the SSI of IMX6, now I have a problem.
When playing a 1KHZ sine wave, there is always a noise.

The software dumps the data in the HAL layer, the data is not abnormal,
the hardware also records the data output by IIS, forms a table, restores the data,
and the waveform is not abnormal.

Doubtful point: The frequency of measuring lrclk cannot be stabilized at 44.1K,
about 43.6xxKHz. Can this be optimized, let SSI lrclk stabilize at 44.1K,
the hardware is actually doing cross-over experiment, and the SOC output
of other models is 1KHZ is connected to our DSP, there is no noise, the
difference is on lrclk, so the hardware suspects that this clock causes the
DSP's digital-to-analog conversion to be abnormal.
IMX6 SSI--------DSP has noise
Other SOC IIS signals fly to -----" DSP has no noise
Looking forward to your reply, thank you!

----------------------------------

Hi lou

one can try to rebuild all image from scratch using nxp linux from

codeaurora.org/external/imx/linux-imx repository

linux-imx - i.MX Linux kernel 

linux documentation

i.MX Software | NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos