IMX6烧写失败

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6烧写失败

816 Views
851334238
Contributor I

你好,

         最近有一块PCBA板,之前使用一直正常,但是昨天发现系统无法启动,接上调试串口,也无启动信息。重新烧写系统镜像,发现无法烧录,下图为烧写工具打印的错误,麻烦帮忙分析一下,谢谢!IMG_1680.JPG

0 Kudos
1 Reply

565 Views
igorpadykov
NXP Employee
NXP Employee

Q: Hello, recently there is a PCBA board, it has been normal use before, but yesterday found that the system does not start, connect the serial debugging, and no start-up information. Re-program the system image, found it impossible to burn, the next picture shows the wrong programming tools to print, trouble to help analyze, thank you!

A:

first please run ddr test to check if that was not caused by ddr failures

https://community.freescale.com/docs/DOC-105652 

use i.MX6 System Development User’s Guide Chapter 8 Avoiding Board Bring-up Problems

http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf

then please try to run linux with minimal configuration

i.MX 6 Series Software and Development Tool|NXP 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos