IMX53QSB don't boot.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX53QSB don't boot.

786 Views
segeypopov
Contributor I

Hello!

Any time ago i bought imx53qsb.

i connect 5V Power adapter, connect VGA monitor, insert the micro SD with default UBUNTU and press POWER.

All led lit. But monitor is black :(

Please tell my about how i can boot device?

Labels (1)
0 Kudos
Reply
1 Reply

729 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sergey

one can prepare new card using below links

Board Support Packages (8)

File and Instructions to create an SD with an Ubuntu Demo Image like the one

provided with the QSB. Supports MCIMX53-START and MCIMX53-START-R. (REV 11.09)

or

Recommended Software & Tools (1)

Linux Binary Demo Files 11.09 Release (REV 2011.09)

http://www.nxp.com/products/interface-and-connectivity/interface-and-system-management/switch-monito...

note there are versions QSB with DA9053,MC34708,MC34709 PMICs, all

use different images, so be careful and read documentation in software packages

on that link.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply