IMX53 with external USB phy via ULPI bus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX53 with external USB phy via ULPI bus

1,600 次查看
jomeke
Contributor II

Hi all,

I am planning to use the IMX537 with a external USB phy connected on USB_HOST3

The used phy is from Texas Instruments "TUSB1210" and is connected to the IMX via the ULPI bus.

The clock pin on the TUSB1210 can be input or output but what about the IXM side ? in de manual IMX53IEC.PDF the pin CSIO_DAT6 is only noted as input.

Is it possible the use the CSIO_DAT6 pin as clock output ?

Regards

Johan

标签 (1)
0 项奖励
回复
3 回复数

1,412 次查看
Yuri
NXP Employee
NXP Employee

yes

0 项奖励
回复

1,412 次查看
jomeke
Contributor II

do you mean that the IMX pin only can be input, that the phy must make the clock signal ?

0 项奖励
回复

1,412 次查看
Yuri
NXP Employee
NXP Employee

The i.MX53 does not support the Clock Input mode of ULPI PHY.

0 项奖励
回复