IMX53 u-boot from NAND, how to debug with lauterbach

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX53 u-boot from NAND, how to debug with lauterbach

2,864 次查看
cristiansicilia
Contributor III

Hello,

I have a IMX53 board, based on loco with a NAND.

I need to boot from NAND, but have some problem, and it don't work.

I would try to debug IMX ROM Bootloader with lauterbah due to verify if the NAND work good or there are some compatibility issue, (I know that it work good on linux, because starting from SD, I can use NAND as rootfs, etc).

There is something that help to do this operation? (like some source to load, the starting address, .. anything that help, I'm really frustrated about that).

My issue is explained here:

IMX53 Loco based board with MT29F8G08ABABA as NFC 8bit

and this is a really similar issue:

How to boot i.MX53 from Nand?

Regards

标签 (2)
标记 (3)
0 项奖励
回复
3 回复数

2,217 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Cristian

MT29F8G08ABABA has 224 byte spare size and formally

is not supported by ROM for boot (max. supported 4KB + 218 Bytes).

Still one can try with setting BOOT_CFG2[7:6]="4KB + 218 Bytes" .

NAND FCB can be written only with kobs-ng tool and

easy way to make bootable NAND image is to use MFG Tool IMX_MFG_TOOL ,

refer to attached ucl.xml file with profile: LIST name="MX53ARD-NAND(JFFS2) .

README_MX53_NAND_BOOT.pdf describes changes

needed for support NAND uboot, these patches are already included

in FSL ltib i.MX53 releases L2.6.35_11_09_ER_SOURCE, for correct

bulding one needs to select "mx53_ard" for uboot building. In general one

can also try kobs-ng from i.MX6 BSP releases, it supports more NAND configurations.

One can try to debug checking NAND signals by oscilloscope,

image header should appear in NFC RAM buffer (then ROM reads it

to iRAM 0xf8006400) - this can be checked with jtag. Note i.MX53

NFC controller supports max.16 bit ECC, NANDs required more ECC

bits are not supported.

Best regards

igor

2,217 次查看
cristiansicilia
Contributor III

Hello *,

I'm trying to debug imx53 in early stage, but seems that the ROM loader get some issue, the code run in loop in memory at 40xxxxh and in Bxxh, so as in the IMX53RM.pdf page 483, at c0h-3fffh and 400000h-40bffh there is the ROM Bootstrap.

lauterback-0x40433C-rom.png

With the scope I see some data on NAND bus.

I tried also to follow this guide, with this u-boot (2014-10) code:

http://www.denx-cs.de/doku/?q=m53evkcompileinstalluboot

after this I use this command (whit my kernel that work good with nand):

umount /dev/mtdblock*

umount /rwfs/

ubidetach -d 5 /dev/ubi_ctrl

mount

mount /dev/mmcblk0p3 /mnt/cdrom/

sleep 3

echo 1 > /sys/devices/platform/mxc_nandv2_flash.0/ignorebad

kobs-ng init -v  /mnt/cdrom/u-boot-with-nand-spl.imx

echo 1 > /sys/devices/platform/mxc_nandv2_flash.0/ignorebad

In the first part I umount all nand partition, mount external sdcard, where is located nand-spl.

My nand is also on PATA pins, the only change is that my UART is on UART1, so I changed the iomux.

0 项奖励
回复

2,217 次查看
skrausse
Contributor II

Hello Cristian,


At least you should try to sue this sequence to connect to the baord:

  SYStem.RESet

  SYStem.CPU IMX535

  SYStem.Option ResBreak OFF

  SYStem.Option WaitReset 100ms

  SYStem.Up

The chip does not allow to connect to the board in an early boot stage, because the debugger has to wait, till the debug clocks internaly are enabled. Important at this stage is, that they later will nto be disabled again by the bootloader (there were some versions, were debug debug port was disablked completely).

If this is not working, then it would be good to know, what error messages you get. You can try to connect in a later boot stage using Attach instead of Up, just to see, if debugging is possible at all. If you were not able to connect in any case, then you could try to select a different boot mode, just for testing.

Best Regards,

Steffen.

0 项奖励
回复