IMX53+WINCE7 strange issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

IMX53+WINCE7 strange issue

跳至解决方案
1,933 次查看
wangweijun
Contributor I

Dear Experts,

We reference IMX53 SMD WINCE7 and developed,now encountered two problems

1.RTC clock

System up,Serial debugging information can look RTC,and run,but taskbar can not look the time,Go to Control Panel>Date and Time,serial debugging infomation below

 

PID:05670BE2 TID:052214B2 Exception 'Raised Exception' (0xc0000094): Thread-Id=052214b2(pth=c082a000), Proc-Id=05670be2(pprc=c08ac000) 'CTLPNL.EXE', VM-active=05670be2(pprc=c08ac000) 'CTLPNL.EXE'

PID:05670BE2 TID:052214B2 PC=40051a94(coredll.dll+0x00041a94) RA=802292cc(kernel.dll+0x0000e2cc) SP=0016eccc, BVA=00000000

PID:00400002 TID:052214B2 Exception 'Raised Exception' (0x116): Thread-Id=052214b2(pth=c082a000), Proc-Id=00400002(pprc=84ea95e0) 'NK.EXE', VM-active=05670be2(pprc=c08ac000) 'CTLPNL.EXE'

PID:00400002 TID:052214B2 PC=eff5f9d4(k.coredll.dll+0x0001f9d4) RA=802292cc(kernel.dll+0x0000e2cc) SP=dc63e7a0, BVA=ffffffff

2.system

Do not know where the reason,the system is HIVE,System starts from emmc(emmc connect SD1,4bit),system up ,can look the letter of MMCMemory,copy a application  of test database into the MMCmemory and run,the application can creat a file and can look the ico,but refresh,the ico is dispappear ,it seem the file is virtual.can't link the file

But if copy the application of test database into the system folder(ie. My Documents) and run ,the application can creat a file and can look two ico,refresh,leave one ico,can link the file.

If copy or cut a file from one folder to other any more folder ,can creat two ico,refresh ,leave one ico.if delete one file,the file ico still ,refresh,the ico disappear.

Problem has plagued us for a long time, do not know how to solve it, thank you very much

标签 (2)
0 项奖励
回复
1 解答
1,389 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

there is  a  fix in Linux  for this case  but   there is no plan/date    yet to solve it in Wince

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,390 次查看
karina_valencia
NXP Apps Support
NXP Apps Support

there is  a  fix in Linux  for this case  but   there is no plan/date    yet to solve it in Wince

0 项奖励
回复