IMX53 QSB interface with OV5640

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX53 QSB interface with OV5640

2,828 次查看
Saminath
Contributor I

IMX53 QSB board interfaced with the OV5640 Sensor interface, I configured boundary_camera and ov5640 driver and Boot Sequence for ov560 are configured. But OV5640 is not responding any of the I2C commands. Any one Faced this issue, kindly response.

标记 (2)
0 项奖励
回复
6 回复数

2,501 次查看
CINCINATO
Contributor I

How did you capture jpeg image?! With gstreamer + v4l2src?

I'm having some trouble with this too.

0 项奖励
回复

2,501 次查看
Saminath
Contributor I

Hi,

Now I able to capture images in Jpeg. Now I am facing one issue on Interrupt Handling in IPU Block. I am able to configure only EOF DMA channels(INT-0). So i will get interrupt notification only After DMA Buffer Full. But I should get the Interrupt Notification at the End-Of-Frame, that is end-of-vsync. Any one attempt on the same. kindly response me.


Thanks in Advance.
sami

0 项奖励
回复

2,501 次查看
daiane_angolini
NXP Employee
NXP Employee

great!

0 项奖励
回复

2,501 次查看
Saminath
Contributor I

Hi ,

Thanks for Reply. For me start working. Two Problems.

1. Boot Sequence was wrong. I corrected it.

2. Hardware connection was wrong in DVDD.

Now It is responding with I2C communication.

0 项奖励
回复

2,501 次查看
daiane_angolini
NXP Employee
NXP Employee

Have you turned on the clock?

0 项奖励
回复

2,501 次查看
haitao
Contributor II

i have same problem! , we can discuss it

0 项奖励
回复