IMX53 QSB interface with OV5640

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX53 QSB interface with OV5640

2,380件の閲覧回数
Saminath
Contributor I

IMX53 QSB board interfaced with the OV5640 Sensor interface, I configured boundary_camera and ov5640 driver and Boot Sequence for ov560 are configured. But OV5640 is not responding any of the I2C commands. Any one Faced this issue, kindly response.

タグ(2)
0 件の賞賛
返信
6 返答(返信)

2,053件の閲覧回数
CINCINATO
Contributor I

How did you capture jpeg image?! With gstreamer + v4l2src?

I'm having some trouble with this too.

0 件の賞賛
返信

2,053件の閲覧回数
Saminath
Contributor I

Hi,

Now I able to capture images in Jpeg. Now I am facing one issue on Interrupt Handling in IPU Block. I am able to configure only EOF DMA channels(INT-0). So i will get interrupt notification only After DMA Buffer Full. But I should get the Interrupt Notification at the End-Of-Frame, that is end-of-vsync. Any one attempt on the same. kindly response me.


Thanks in Advance.
sami

0 件の賞賛
返信

2,053件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

great!

0 件の賞賛
返信

2,053件の閲覧回数
Saminath
Contributor I

Hi ,

Thanks for Reply. For me start working. Two Problems.

1. Boot Sequence was wrong. I corrected it.

2. Hardware connection was wrong in DVDD.

Now It is responding with I2C communication.

0 件の賞賛
返信

2,053件の閲覧回数
daiane_angolini
NXP Employee
NXP Employee

Have you turned on the clock?

0 件の賞賛
返信

2,053件の閲覧回数
haitao
Contributor II

i have same problem! , we can discuss it

0 件の賞賛
返信