Hello,
I have a board with an SD card and an MMC on board. The SD card work good, but with MMC I have some problem. U-Boot list the MMC but can't do anything on it:
I2C: ready
DRAM: 512 MB
MMC: FSL_ESDHC: 0,FSL_ESDHC: 1
In: serial
Out: serial
Err: serial
i2c: I2C3 SDA is low, start i2c recovery...
I2C3 Recovery success
Serial reinitilized!
Net: No ethernet found.
Hit any key to stop autoboot: 0
...
U-Boot>
mmc dev 1
mmc1(part 0) is current device
U-Boot> mmc part
## Unknown partition table
mmc read ${loadaddr} 0 1
MMC read: dev # 1, block # 0, count 1 ... MMC: block number 0x1 exceeds max(0x0)
0 blocks read: ERROR
I'm sure that the mmc have a partion, I have done it from kernel (where the mmc work good).
I have this MMC:
The config is:
#ifdef CONFIG_CMD_MMC
#define CONFIG_MMC 1
#define CONFIG_GENERIC_MMC
#define CONFIG_IMX_MMC
#define CONFIG_SYS_FSL_ESDHC_NUM 2
#define CONFIG_SYS_FSL_ESDHC_ADDR 0
#define CONFIG_SYS_MMC_ENV_DEV 0
#define CONFIG_DOS_PARTITION 1
#define CONFIG_CMD_FAT 1
#define CONFIG_CMD_EXT2 1
/* detect whether ESDHC1 or ESDHC3 is boot device */
#define CONFIG_DYNAMIC_MMC_DEVNO
#define CONFIG_EMMC_DDR_PORT_DETECT
#define CONFIG_EMMC_DDR_MODE
/* port 1 (ESDHC3) is 8 bit */
#define CONFIG_MMC_8BIT_PORTS 0x2
#endif
The for esdhc_gpio_init is:
struct fsl_esdhc_cfg esdhc_cfg[2] = {
{MMC_SDHC1_BASE_ADDR, 1, 1},
{MMC_SDHC3_BASE_ADDR, 1, 1},
};
int esdhc_gpio_init(bd_t *bis)
{
s32 status = 0;
mxc_request_iomux(MX53_PIN_SD1_CMD, IOMUX_CONFIG_ALT0);
mxc_request_iomux(MX53_PIN_SD1_CLK, IOMUX_CONFIG_ALT0);
mxc_request_iomux(MX53_PIN_SD1_DATA0,
IOMUX_CONFIG_ALT0);
mxc_request_iomux(MX53_PIN_SD1_DATA1,
IOMUX_CONFIG_ALT0);
mxc_request_iomux(MX53_PIN_SD1_DATA2,
IOMUX_CONFIG_ALT0);
mxc_request_iomux(MX53_PIN_SD1_DATA3,
IOMUX_CONFIG_ALT0);
mxc_iomux_set_pad(MX53_PIN_SD1_CMD, 0x1E4);
mxc_iomux_set_pad(MX53_PIN_SD1_CLK, 0xD4);
mxc_iomux_set_pad(MX53_PIN_SD1_DATA0, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_SD1_DATA1, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_SD1_DATA2, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_SD1_DATA3, 0x1D4);
status |= fsl_esdhc_initialize(bis, &esdhc_cfg[0]);
mxc_request_iomux(MX53_PIN_ATA_RESET_B, IOMUX_CONFIG_ALT2);
mxc_request_iomux(MX53_PIN_ATA_IORDY, IOMUX_CONFIG_ALT2);
mxc_request_iomux(MX53_PIN_ATA_DA_0, IOMUX_CONFIG_ALT2);
mxc_request_iomux(MX53_PIN_ATA_DATA8, IOMUX_CONFIG_ALT4);
mxc_request_iomux(MX53_PIN_ATA_DATA9, IOMUX_CONFIG_ALT4);
mxc_request_iomux(MX53_PIN_ATA_DATA10, IOMUX_CONFIG_ALT4);
mxc_request_iomux(MX53_PIN_ATA_DATA11, IOMUX_CONFIG_ALT4);
mxc_request_iomux(MX53_PIN_ATA_DATA0, IOMUX_CONFIG_ALT4);
mxc_request_iomux(MX53_PIN_ATA_DATA1, IOMUX_CONFIG_ALT4);
mxc_request_iomux(MX53_PIN_ATA_DATA2, IOMUX_CONFIG_ALT4);
mxc_request_iomux(MX53_PIN_ATA_DATA3, IOMUX_CONFIG_ALT4);
mxc_iomux_set_pad(MX53_PIN_ATA_DA_0, 0x1E4);
mxc_iomux_set_pad(MX53_PIN_ATA_RESET_B, 0x1E4);
mxc_iomux_set_pad(MX53_PIN_ATA_IORDY, 0xD4);
mxc_iomux_set_pad(MX53_PIN_ATA_DATA8, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_ATA_DATA9, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_ATA_DATA10, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_ATA_DATA11, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_ATA_DATA0, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_ATA_DATA1, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_ATA_DATA2, 0x1D4);
mxc_iomux_set_pad(MX53_PIN_ATA_DATA3, 0x1D4);
status |= fsl_esdhc_initialize(bis, &esdhc_cfg[1]);
return status;
}
Have any suggestion?
Hi Cristian
this error may be caused by wrong image, generated for
other board. Had you tried with FSL BSP
L2.6.35_11_09_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation
11.09. Supports MCIMX53-START and MCIMX53-START-R.
L2.6.35_11.05_ER_SOURCE : Linux 2.6.35 Source Code Files and documentation
11.05 for i.MX53 SABRE Tablet.
Best regards
igor
Hello,
I'm not sure if I understand your suggestion.
I have a custom board, based on LOCO (one ram bank etc), but there is mounted on an MMC as in the schematic posted.
I tried all u-boot present in MFGTOOL profiles, but only loco start, but the emmc don't work.
The IMX connection to MMC are:
And is really close to quick start board:
The Quick start board mount an mmc, and have WP and CD pins.
Regards
I would suggest to check if emmc is working at all with standalone test
IMX53_QSB_OBDS "On-Board Diagnostic Suit for the i.MX53 Quick Start Board"
http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB&fpsp=1&tab=Design_Tools_Tab
Best regards
igor
Thank you,
I try it now!
But when I start linux kernel (loading it from SD CARD), I can manage the internal emmc normally
// SDCARD
mmcblk0: mmc0:aaaa SU08G 7.40 GiB
mmcblk0:
p1 p2 p3
// internal eMMC
mmc1: new high speed MMC card at address 0001
mmcblk1: mmc1:0001 002G49 1.82 GiB
mmcblk1:
p1
// And do some operation on it
root@nsip ~$ mount /dev/mmcblk1p1 /mnt/cdrom/
root@nsip ~$ ls /mnt/cdrom/
ciao lost+found
root@nsip ~$ echo vvvv > /mnt/cdrom/test
root@nsip ~$ umount /mnt/cdrom/
root@nsip ~$ mount /dev/mmcblk1p1 /mnt/cdrom/
root@nsip ~$ ls /mnt/cdrom/
ciao lost+found test
root@nsip ~$ cat /mnt/cdrom/test
vvvv
root@nsip ~$
I tryed to enable trace in U-BOOT:
U-BOOT> mmc dev 1
CMD_SEND:0
ARG 0x00000000
FLAG 0
MMC_RSP_NONE
CMD_SEND:8
ARG 0x000001AA
FLAG 0
MMC_RSP_R1,5,6,7 0x00000000
CMD_SEND:55
ARG 0x00000000
FLAG 0
MMC_RSP_R1,5,6,7 0xFFFFFFFF
CMD_SEND:0
ARG 0x00000000
FLAG 0
MMC_RSP_NONE
CMD_SEND:1
ARG 0x00000000
FLAG 0
MMC_RSP_R3,4 0x007F8000
CMD_SEND:1
ARG 0x40360000
FLAG 0
MMC_RSP_R3,4 0x007F8000
CMD_SEND:1
ARG 0x40360000
FLAG 0
FLAG 0
MMC_RSP_R3,4 0x007F8000
CMD_SEND:1
ARG 0x40360000
FLAG 0
MMC_RSP_R3,4 0x007F8000
CMD_SEND:1
ARG 0x40360000
FLAG 0
MMC_RSP_R3,4 0x807F8000
CMD_SEND:2
ARG 0x00000000
FLAG 0
MMC_RSP_R2 0x774FFB4C
0x774FFB70
0x778067BC
0x778219EE
DUMPING DATA
000 - 77 4F FB 4C
004 - 77 4F FB 70
008 - 77 80 67 BC
012 - 77 82 19 EE
mmc1(part 0) is current device
U-BOOT>
I tried to do the mmcinfo on eMMC, but I get only 0:
Device: FSL_ESDHC
Manufacturer ID: 0
OEM: 0
Name: Tran Speed: 0
Rd Block Len: 0
MMC version 0.0
High Capacity: No
Capacity: 0 Bytes
Bus Width: 1-bit
Current Partition for boot: Not bootable
And analyzing the SEND_CMD:2 dump:
- 000 - 77 4F FB 4C
- 004 - 77 4F FB 70
- 008 - 77 80 67 BC
- 012 - 77 82 19 EE
seems don't match with the eMMC datasheet (attached).
With this command I get an error:
U-BOOT> mmc dev 2
MMC Device 2 not found
no mmc device at slot 2
Consider that this is a IM53 not an IMX6.
And when I reset it show:
...
Boot Device: SD
I2C: ready
DRAM: 512 MB
MMC: FSL_ESDHC: 0,FSL_ESDHC: 1
...
And the fsl struct is:
- struct fsl_esdhc_cfg esdhc_cfg[2] = {
- {MMC_SDHC1_BASE_ADDR, 1, 1},
- {MMC_SDHC3_BASE_ADDR, 1, 1},
- };
I tried to add the SDCH2 due to shift dev to 2, but the result is the same.
Also using the u-boot for loco board in mfgtool the read on internal mmc don't work.
Any other suggestion?
Consider that:
A - The u-boot on eMMC is loaded correctly by the IMX53 ROM loader
B - The eMMC is used successfully with the kernel
Regards