HI,
I try to use kernel 3.11 rc4 on the imx53 loco board.
To configure the hw I use the: imx53-qsb.dts
The kernel work correctly. I have congured and tested the VGA and LVDS.
Now I try to use the USB Host, but when I attach something the kernel do nothing.
For example I attach a USB-Mouse and the light of the mouse flash for 100 ms and the kernel do nothing. Idem with a USB Mass Storage.
Can You Help ME.
Best Regards
Domenico
解決済! 解決策の投稿を見る。
Hi Domenico,
I fixed the USBH1 issue on mx53qsb with the mainline kernel.
You will need these two patches:
and
(If you use linux-next 20132208 it contains both patches already)
Also, currently only mx53qsb with Dialog PMIC will work with USBH1. The mx53qsb with mc34708 pmic will not have USBHost functional because the VBUS is supplied from the pmic and this pmic is not supported yet (I plan to submit mc34708 regulator support soon).
As a workaround you can activate the pmic via U-boot (usb reset) as a workaround.
Regards,
Fabio Estevam
Hello Domenico,
how did you get vga working with the 3.11 kernel?
Thanks in advance,
Roel
For TVE funcionality on mx53qsb with mainline kernel, you need to apply this patch that has been recently submitted:
[PATCH 2/2] ARM i.MX53: dts: Add TVE to i.MX53-QSB device tree
Hi Domenico,
I fixed the USBH1 issue on mx53qsb with the mainline kernel.
You will need these two patches:
and
(If you use linux-next 20132208 it contains both patches already)
Also, currently only mx53qsb with Dialog PMIC will work with USBH1. The mx53qsb with mc34708 pmic will not have USBHost functional because the VBUS is supplied from the pmic and this pmic is not supported yet (I plan to submit mc34708 regulator support soon).
As a workaround you can activate the pmic via U-boot (usb reset) as a workaround.
Regards,
Fabio Estevam
I just want to remind i.MX53 QSB USB connectors specific :
"The Lower USB Host Jack and the Micro USB Device Jack are cross connected.
[BOTTOM USB HOST SHARED WITH USB DEVICE.] The user can plug one cable into
either jack, but cannot plug cables into both jacks at the same time."
For Host it makes sense to use UPPER USB connector.
We have BSP for the i.MX53QSB. You can download it from here:
<https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=IMX53QSB>
The version is L2.6.35_11_09_ER_SOURCE. It is well tested for i.MX53QSB. Please try it.
And please also apply the patch. IMX53_LINUX_1109_BSP_PATCH