IMX515 optimization

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMX515 optimization

3,434件の閲覧回数
Misan
Contributor I

hi, i am working on IMX515(CORTEX A8) processor. We have  ported one image processing algorithm but it runs very slowly so i request you all please give some basic ideas about the optimization.

 

1. as i read cortex a8 has 13 stage pipeline . but i would like to have the pipeline information .

gcc compiler doesnt give any info regarding this.

2. I guess it has SDMA . how to implement this sdma. i would like to send the data from external memory to internal memory.

 

3. I tried the NEON but as my code doesnt have any serial excution so it doesnt give the good performance.

 

if any one has any idea regarding the above question, please reply at your convenience

タグ(1)
0 件の賞賛
返信
2 返答(返信)

3,086件の閲覧回数
LyonWang
NXP Employee
NXP Employee

Another tips: please make sure L2 cache is enabled, cause NEON processor need L2 cache for Instruction and Data.

And attached some useful arm NEON reference document FYI

0 件の賞賛
返信

3,086件の閲覧回数
JerryFan
NXP Employee
NXP Employee

1. You can find the information about cortex a8 pipeline on arm's website. But I think the pipeline should be transparent to SW.

2. Yes, it has SDMA. I think in your case, a memory-2-memory transfer should be OK. But the SDMA core works at about 60MHz, so the data rate will not be very high. 

3. Even your code have no any serial execution, the NEON should give a performance improvement. Please refer http://infocenter.arm.com/help/topic/com.arm.doc.ddi0344i/Chddgcfe.html to know how to take the advantage of NEON.

4. Make sure you code has a good cache hit rate. It is important. 

5. The critical function should be written in assemble and optimized carefully.

0 件の賞賛
返信