IMX35 UDC driver init issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX35 UDC driver init issue

Jump to solution
2,308 Views
benoysaha
Contributor II


Hello ,

I am using a customized board with imx35 and porting 2.6.31 linux to it. For reference i have taken the linux code from 2.6.31 PDK source for freescale imx35 s stack board. I could bring up the board with basic drivers and now i want to use this board as USB gadget.

I have seen some issue in initializing the Usb Device controller driver. I could see that drivers/usb/gadget/fsl_udc_core.c -> udc_init() returns with error with value -19.

Here is my .config file -

#
# Automatically generated make config: don't edit
# Linux kernel version: 2.6.31
# Mon Mar  4 06:19:20 2013
#
CONFIG_ARM=y
CONFIG_SYS_SUPPORTS_APM_EMULATION=y
CONFIG_GENERIC_GPIO=y
CONFIG_GENERIC_TIME=y
CONFIG_GENERIC_CLOCKEVENTS=y
CONFIG_MMU=y
CONFIG_GENERIC_HARDIRQS=y
CONFIG_STACKTRACE_SUPPORT=y
CONFIG_HAVE_LATENCYTOP_SUPPORT=y
CONFIG_LOCKDEP_SUPPORT=y
CONFIG_TRACE_IRQFLAGS_SUPPORT=y
CONFIG_HARDIRQS_SW_RESEND=y
CONFIG_GENERIC_IRQ_PROBE=y
CONFIG_RWSEM_GENERIC_SPINLOCK=y
CONFIG_GENERIC_HWEIGHT=y
CONFIG_GENERIC_CALIBRATE_DELAY=y
CONFIG_ZONE_DMA=y
CONFIG_ARCH_MTD_XIP=y
CONFIG_GENERIC_HARDIRQS_NO__DO_IRQ=y
CONFIG_OPROFILE_ARMV6=y
CONFIG_OPROFILE_ARM11_CORE=y
CONFIG_VECTORS_BASE=0xffff0000
CONFIG_DEFCONFIG_LIST="/lib/modules/$UNAME_RELEASE/.config"
CONFIG_CONSTRUCTORS=y

#
# General setup
#
CONFIG_EXPERIMENTAL=y
CONFIG_BROKEN_ON_SMP=y
CONFIG_LOCK_KERNEL=y
CONFIG_INIT_ENV_ARG_LIMIT=32
CONFIG_LOCALVERSION=""
CONFIG_LOCALVERSION_AUTO=y
CONFIG_SWAP=y
CONFIG_SYSVIPC=y
CONFIG_SYSVIPC_SYSCTL=y
# CONFIG_POSIX_MQUEUE is not set
# CONFIG_BSD_PROCESS_ACCT is not set
# CONFIG_TASKSTATS is not set
# CONFIG_AUDIT is not set

#
# RCU Subsystem
#
CONFIG_CLASSIC_RCU=y
# CONFIG_TREE_RCU is not set
# CONFIG_PREEMPT_RCU is not set
# CONFIG_TREE_RCU_TRACE is not set
# CONFIG_PREEMPT_RCU_TRACE is not set
CONFIG_IKCONFIG=y
CONFIG_IKCONFIG_PROC=y
CONFIG_LOG_BUF_SHIFT=14
# CONFIG_GROUP_SCHED is not set
# CONFIG_CGROUPS is not set
CONFIG_SYSFS_DEPRECATED=y
CONFIG_SYSFS_DEPRECATED_V2=y
# CONFIG_RELAY is not set
# CONFIG_NAMESPACES is not set
CONFIG_BLK_DEV_INITRD=y
CONFIG_INITRAMFS_SOURCE=""
CONFIG_RD_GZIP=y
# CONFIG_RD_BZIP2 is not set
# CONFIG_RD_LZMA is not set
CONFIG_CC_OPTIMIZE_FOR_SIZE=y
CONFIG_SYSCTL=y
CONFIG_ANON_INODES=y
CONFIG_EMBEDDED=y
CONFIG_UID16=y
CONFIG_SYSCTL_SYSCALL=y
CONFIG_KALLSYMS=y
# CONFIG_KALLSYMS_ALL is not set
# CONFIG_KALLSYMS_EXTRA_PASS is not set
CONFIG_HOTPLUG=y
CONFIG_PRINTK=y
CONFIG_BUG=y
CONFIG_ELF_CORE=y
CONFIG_BASE_FULL=y
CONFIG_FUTEX=y
CONFIG_EPOLL=y
CONFIG_SIGNALFD=y
CONFIG_TIMERFD=y
CONFIG_EVENTFD=y
CONFIG_SHMEM=y
CONFIG_AIO=y

#
# Performance Counters
#
CONFIG_VM_EVENT_COUNTERS=y
CONFIG_SLUB_DEBUG=y
# CONFIG_STRIP_ASM_SYMS is not set
CONFIG_COMPAT_BRK=y
# CONFIG_SLAB is not set
CONFIG_SLUB=y
# CONFIG_SLOB is not set
CONFIG_PROFILING=y
CONFIG_TRACEPOINTS=y
CONFIG_MARKERS=y
CONFIG_OPROFILE=y
CONFIG_HAVE_OPROFILE=y
# CONFIG_KPROBES is not set
CONFIG_HAVE_KPROBES=y
CONFIG_HAVE_KRETPROBES=y

#
# GCOV-based kernel profiling
#
# CONFIG_GCOV_KERNEL is not set
# CONFIG_SLOW_WORK is not set
CONFIG_HAVE_GENERIC_DMA_COHERENT=y
CONFIG_SLABINFO=y
CONFIG_RT_MUTEXES=y
CONFIG_BASE_SMALL=0
CONFIG_MODULES=y
# CONFIG_MODULE_FORCE_LOAD is not set
CONFIG_MODULE_UNLOAD=y
CONFIG_MODULE_FORCE_UNLOAD=y
CONFIG_MODVERSIONS=y
# CONFIG_MODULE_SRCVERSION_ALL is not set
CONFIG_BLOCK=y
CONFIG_LBDAF=y
# CONFIG_BLK_DEV_BSG is not set
# CONFIG_BLK_DEV_INTEGRITY is not set

#
# IO Schedulers
#
CONFIG_IOSCHED_NOOP=y
CONFIG_IOSCHED_AS=y
CONFIG_IOSCHED_DEADLINE=y
CONFIG_IOSCHED_CFQ=y
# CONFIG_DEFAULT_AS is not set
# CONFIG_DEFAULT_DEADLINE is not set
CONFIG_DEFAULT_CFQ=y
# CONFIG_DEFAULT_NOOP is not set
CONFIG_DEFAULT_IOSCHED="cfq"
CONFIG_FREEZER=y

#
# System Type
#
# CONFIG_ARCH_AAEC2000 is not set
# CONFIG_ARCH_INTEGRATOR is not set
# CONFIG_ARCH_REALVIEW is not set
# CONFIG_ARCH_VERSATILE is not set
# CONFIG_ARCH_AT91 is not set
# CONFIG_ARCH_CLPS711X is not set
# CONFIG_ARCH_GEMINI is not set
# CONFIG_ARCH_EBSA110 is not set
# CONFIG_ARCH_EP93XX is not set
# CONFIG_ARCH_FOOTBRIDGE is not set
CONFIG_ARCH_MXC=y
# CONFIG_ARCH_STMP3XXX is not set
# CONFIG_ARCH_NETX is not set
# CONFIG_ARCH_H720X is not set
# CONFIG_ARCH_IOP13XX is not set
# CONFIG_ARCH_IOP32X is not set
# CONFIG_ARCH_IOP33X is not set
# CONFIG_ARCH_IXP23XX is not set
# CONFIG_ARCH_IXP2000 is not set
# CONFIG_ARCH_IXP4XX is not set
# CONFIG_ARCH_L7200 is not set
# CONFIG_ARCH_KIRKWOOD is not set
# CONFIG_ARCH_LOKI is not set
# CONFIG_ARCH_MV78XX0 is not set
# CONFIG_ARCH_ORION5X is not set
# CONFIG_ARCH_MMP is not set
# CONFIG_ARCH_KS8695 is not set
# CONFIG_ARCH_NS9XXX is not set
# CONFIG_ARCH_W90X900 is not set
# CONFIG_ARCH_PNX4008 is not set
# CONFIG_ARCH_PXA is not set
# CONFIG_ARCH_MSM is not set
# CONFIG_ARCH_RPC is not set
# CONFIG_ARCH_SA1100 is not set
# CONFIG_ARCH_S3C2410 is not set
# CONFIG_ARCH_S3C64XX is not set
# CONFIG_ARCH_SHARK is not set
# CONFIG_ARCH_LH7A40X is not set
# CONFIG_ARCH_U300 is not set
# CONFIG_ARCH_DAVINCI is not set
# CONFIG_ARCH_OMAP is not set
CONFIG_DMA_ZONE_SIZE=24

#
# Freescale MXC Implementations
#
# CONFIG_ARCH_MX1 is not set
# CONFIG_ARCH_MX2 is not set
# CONFIG_ARCH_MX3 is not set
# CONFIG_ARCH_MX25 is not set
CONFIG_ARCH_MX35=y
# CONFIG_ARCH_MX37 is not set
# CONFIG_ARCH_MX51 is not set
CONFIG_MXC_SDMA_API=y
CONFIG_SDMA_IRAM=y
CONFIG_SDMA_IRAM_SIZE=0x1000
CONFIG_ARCH_MXC_HAS_NFC_V2=y
CONFIG_I2C_MXC_SELECT1=y
# CONFIG_I2C_MXC_SELECT2 is not set
# CONFIG_I2C_MXC_SELECT3 is not set
CONFIG_ARCH_MXC_HAS_NFC_V2_1=y

#
# MX35 Options
#
CONFIG_FORCE_MAX_ZONEORDER=13
CONFIG_MX35_OPTIONS=y
CONFIG_MACH_MX35_3DS=y
# CONFIG_MACH_MX35EVB is not set
# CONFIG_MX35_DOZE_DURING_IDLE is not set

#
# SDMA options
#

#
# Device options
#
CONFIG_MXC_PSEUDO_IRQS=y
CONFIG_ARCH_HAS_EVTMON=y
# CONFIG_MXC_IRQ_PRIOR is not set
# CONFIG_MXC_PWM is not set
CONFIG_ARCH_HAS_RNGC=y

#
# Processor Type
#
CONFIG_CPU_32=y
CONFIG_CPU_V6=y
# CONFIG_CPU_32v6K is not set
CONFIG_CPU_32v6=y
CONFIG_CPU_ABRT_EV6=y
CONFIG_CPU_PABRT_NOIFAR=y
CONFIG_CPU_CACHE_V6=y
CONFIG_CPU_CACHE_VIPT=y
CONFIG_CPU_COPY_V6=y
CONFIG_CPU_TLB_V6=y
CONFIG_CPU_HAS_ASID=y
CONFIG_CPU_CP15=y
CONFIG_CPU_CP15_MMU=y

#
# Processor Features
#
CONFIG_ARM_THUMB=y
# CONFIG_CPU_ICACHE_DISABLE is not set
# CONFIG_CPU_DCACHE_DISABLE is not set
# CONFIG_CPU_BPREDICT_DISABLE is not set
CONFIG_OUTER_CACHE=y
CONFIG_CACHE_L2X0=y
CONFIG_ARM_ERRATA_411920=y
CONFIG_ARM_ERRATA_364296=y

#
# Bus support
#
# CONFIG_PCI_SYSCALL is not set
# CONFIG_ARCH_SUPPORTS_MSI is not set
# CONFIG_PCCARD is not set

#
# Kernel Features
#
CONFIG_TICK_ONESHOT=y
CONFIG_NO_HZ=y
CONFIG_HIGH_RES_TIMERS=y
CONFIG_GENERIC_CLOCKEVENTS_BUILD=y
CONFIG_VMSPLIT_3G=y
# CONFIG_VMSPLIT_2G is not set
# CONFIG_VMSPLIT_1G is not set
CONFIG_PAGE_OFFSET=0xC0000000
CONFIG_PREEMPT=y
CONFIG_HZ=100
CONFIG_AEABI=y
# CONFIG_OABI_COMPAT is not set
# CONFIG_ARCH_SPARSEMEM_DEFAULT is not set
# CONFIG_ARCH_SELECT_MEMORY_MODEL is not set
# CONFIG_HIGHMEM is not set
CONFIG_SELECT_MEMORY_MODEL=y
CONFIG_FLATMEM_MANUAL=y
# CONFIG_DISCONTIGMEM_MANUAL is not set
# CONFIG_SPARSEMEM_MANUAL is not set
CONFIG_FLATMEM=y
CONFIG_FLAT_NODE_MEM_MAP=y
CONFIG_PAGEFLAGS_EXTENDED=y
CONFIG_SPLIT_PTLOCK_CPUS=4
# CONFIG_PHYS_ADDR_T_64BIT is not set
CONFIG_ZONE_DMA_FLAG=1
CONFIG_BOUNCE=y
CONFIG_VIRT_TO_BUS=y
CONFIG_HAVE_MLOCK=y
CONFIG_HAVE_MLOCKED_PAGE_BIT=y
CONFIG_DEFAULT_MMAP_MIN_ADDR=4096
# CONFIG_LEDS is not set
CONFIG_ALIGNMENT_TRAP=y
# CONFIG_UACCESS_WITH_MEMCPY is not set

#
# Boot options
#
CONFIG_ZBOOT_ROM_TEXT=0x0
CONFIG_ZBOOT_ROM_BSS=0x0
CONFIG_CMDLINE=""
# CONFIG_XIP_KERNEL is not set
# CONFIG_KEXEC is not set

#
# CPU Power Management
#
# CONFIG_CPU_FREQ is not set
# CONFIG_CPU_IDLE is not set

#
# Floating point emulation
#

#
# At least one emulation must be selected
#
CONFIG_VFP=y

#
# Userspace binary formats
#
CONFIG_BINFMT_ELF=y
# CONFIG_CORE_DUMP_DEFAULT_ELF_HEADERS is not set
CONFIG_HAVE_AOUT=y
# CONFIG_BINFMT_AOUT is not set
# CONFIG_BINFMT_MISC is not set

#
# Power management options
#
CONFIG_PM=y
# CONFIG_PM_DEBUG is not set
CONFIG_PM_SLEEP=y
CONFIG_SUSPEND=y
CONFIG_SUSPEND_FREEZER=y
# CONFIG_APM_EMULATION is not set
CONFIG_ARCH_SUSPEND_POSSIBLE=y
CONFIG_NET=y

#
# Networking options
#
# CONFIG_PACKET is not set
# CONFIG_UNIX is not set
# CONFIG_NET_KEY is not set
# CONFIG_INET is not set
# CONFIG_NETWORK_SECMARK is not set
# CONFIG_NETFILTER is not set
# CONFIG_ATM is not set
# CONFIG_BRIDGE is not set
# CONFIG_NET_DSA is not set
# CONFIG_VLAN_8021Q is not set
# CONFIG_DECNET is not set
# CONFIG_LLC2 is not set
# CONFIG_IPX is not set
# CONFIG_ATALK is not set
# CONFIG_X25 is not set
# CONFIG_LAPB is not set
# CONFIG_WAN_ROUTER is not set
# CONFIG_PHONET is not set
# CONFIG_IEEE802154 is not set
# CONFIG_NET_SCHED is not set
# CONFIG_DCB is not set

#
# Network testing
#
# CONFIG_NET_PKTGEN is not set
# CONFIG_HAMRADIO is not set
# CONFIG_CAN is not set
# CONFIG_IRDA is not set
# CONFIG_BT is not set
CONFIG_WIRELESS=y
# CONFIG_CFG80211 is not set
# CONFIG_WIRELESS_OLD_REGULATORY is not set
# CONFIG_WIRELESS_EXT is not set
# CONFIG_LIB80211 is not set

#
# CFG80211 needs to be enabled for MAC80211
#
CONFIG_MAC80211_DEFAULT_PS_VALUE=0
# CONFIG_WIMAX is not set
# CONFIG_RFKILL is not set
# CONFIG_NET_9P is not set

#
# Device Drivers
#

#
# Generic Driver Options
#
CONFIG_UEVENT_HELPER_PATH="/sbin/hotplug"
CONFIG_STANDALONE=y
CONFIG_PREVENT_FIRMWARE_BUILD=y
CONFIG_FW_LOADER=y
CONFIG_FIRMWARE_IN_KERNEL=y
CONFIG_EXTRA_FIRMWARE=""
# CONFIG_DEBUG_DRIVER is not set
# CONFIG_DEBUG_DEVRES is not set
# CONFIG_SYS_HYPERVISOR is not set
# CONFIG_CONNECTOR is not set
CONFIG_MTD=y
# CONFIG_MTD_DEBUG is not set
# CONFIG_MTD_CONCAT is not set
# CONFIG_MTD_PARTITIONS is not set
# CONFIG_MTD_TESTS is not set

#
# User Modules And Translation Layers
#
# CONFIG_MTD_CHAR is not set
# CONFIG_MTD_BLKDEVS is not set
# CONFIG_MTD_BLOCK is not set
# CONFIG_MTD_BLOCK_RO is not set
# CONFIG_FTL is not set
# CONFIG_NFTL is not set
# CONFIG_INFTL is not set
# CONFIG_RFD_FTL is not set
# CONFIG_SSFDC is not set
# CONFIG_MTD_OOPS is not set

#
# RAM/ROM/Flash chip drivers
#
CONFIG_MTD_CFI=y
# CONFIG_MTD_JEDECPROBE is not set
CONFIG_MTD_GEN_PROBE=y
# CONFIG_MTD_CFI_ADV_OPTIONS is not set
CONFIG_MTD_MAP_BANK_WIDTH_1=y
CONFIG_MTD_MAP_BANK_WIDTH_2=y
CONFIG_MTD_MAP_BANK_WIDTH_4=y
# CONFIG_MTD_MAP_BANK_WIDTH_8 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_16 is not set
# CONFIG_MTD_MAP_BANK_WIDTH_32 is not set
CONFIG_MTD_CFI_I1=y
CONFIG_MTD_CFI_I2=y
# CONFIG_MTD_CFI_I4 is not set
# CONFIG_MTD_CFI_I8 is not set
# CONFIG_MTD_CFI_INTELEXT is not set
# CONFIG_MTD_CFI_AMDSTD is not set
# CONFIG_MTD_CFI_STAA is not set
CONFIG_MTD_CFI_UTIL=y
# CONFIG_MTD_RAM is not set
# CONFIG_MTD_ROM is not set
# CONFIG_MTD_ABSENT is not set

#
# Mapping drivers for chip access
#
# CONFIG_MTD_COMPLEX_MAPPINGS is not set
# CONFIG_MTD_PHYSMAP is not set
# CONFIG_MTD_ARM_INTEGRATOR is not set
# CONFIG_MTD_PLATRAM is not set
# CONFIG_MTD_MXC is not set

#
# Self-contained MTD device drivers
#
# CONFIG_MTD_DATAFLASH is not set
# CONFIG_MTD_MXC_DATAFLASH is not set
# CONFIG_MTD_M25P80 is not set
# CONFIG_MTD_SLRAM is not set
# CONFIG_MTD_PHRAM is not set
# CONFIG_MTD_MTDRAM is not set
# CONFIG_MTD_BLOCK2MTD is not set

#
# Disk-On-Chip Device Drivers
#
# CONFIG_MTD_DOC2000 is not set
# CONFIG_MTD_DOC2001 is not set
# CONFIG_MTD_DOC2001PLUS is not set
# CONFIG_MTD_NAND is not set
# CONFIG_MTD_ONENAND is not set

#
# LPDDR flash memory drivers
#
# CONFIG_MTD_LPDDR is not set

#
# UBI - Unsorted block images
#
# CONFIG_MTD_UBI is not set
# CONFIG_PARPORT is not set
CONFIG_BLK_DEV=y
# CONFIG_BLK_DEV_COW_COMMON is not set
CONFIG_BLK_DEV_LOOP=y
# CONFIG_BLK_DEV_CRYPTOLOOP is not set
# CONFIG_BLK_DEV_NBD is not set
CONFIG_BLK_DEV_RAM=y
CONFIG_BLK_DEV_RAM_COUNT=16
CONFIG_BLK_DEV_RAM_SIZE=8192
# CONFIG_BLK_DEV_XIP is not set
# CONFIG_CDROM_PKTCDVD is not set
# CONFIG_ATA_OVER_ETH is not set
# CONFIG_MG_DISK is not set
CONFIG_MISC_DEVICES=y
# CONFIG_ICS932S401 is not set
# CONFIG_ENCLOSURE_SERVICES is not set
# CONFIG_ISL29003 is not set
# CONFIG_C2PORT is not set

#
# EEPROM support
#
# CONFIG_EEPROM_AT24 is not set
# CONFIG_EEPROM_AT25 is not set
# CONFIG_EEPROM_LEGACY is not set
# CONFIG_EEPROM_MAX6875 is not set
# CONFIG_EEPROM_93CX6 is not set
CONFIG_HAVE_IDE=y
# CONFIG_IDE is not set

#
# SCSI device support
#
# CONFIG_RAID_ATTRS is not set
CONFIG_SCSI=y
CONFIG_SCSI_DMA=y
# CONFIG_SCSI_TGT is not set
# CONFIG_SCSI_NETLINK is not set
CONFIG_SCSI_PROC_FS=y

#
# SCSI support type (disk, tape, CD-ROM)
#
CONFIG_BLK_DEV_SD=y
# CONFIG_CHR_DEV_ST is not set
# CONFIG_CHR_DEV_OSST is not set
CONFIG_BLK_DEV_SR=y
# CONFIG_BLK_DEV_SR_VENDOR is not set
# CONFIG_CHR_DEV_SG is not set
# CONFIG_CHR_DEV_SCH is not set
CONFIG_SCSI_MULTI_LUN=y
# CONFIG_SCSI_CONSTANTS is not set
# CONFIG_SCSI_LOGGING is not set
# CONFIG_SCSI_SCAN_ASYNC is not set
CONFIG_SCSI_WAIT_SCAN=m

#
# SCSI Transports
#
# CONFIG_SCSI_SPI_ATTRS is not set
# CONFIG_SCSI_FC_ATTRS is not set
# CONFIG_SCSI_ISCSI_ATTRS is not set
# CONFIG_SCSI_SAS_LIBSAS is not set
# CONFIG_SCSI_SRP_ATTRS is not set
CONFIG_SCSI_LOWLEVEL=y
# CONFIG_LIBFC is not set
# CONFIG_LIBFCOE is not set
# CONFIG_SCSI_DEBUG is not set
# CONFIG_SCSI_DH is not set
# CONFIG_SCSI_OSD_INITIATOR is not set
CONFIG_ATA=m
# CONFIG_ATA_NONSTANDARD is not set
# CONFIG_SATA_PMP is not set
CONFIG_ATA_SFF=y
# CONFIG_SATA_MV is not set
# CONFIG_PATA_PLATFORM is not set
CONFIG_PATA_FSL=m
# CONFIG_MD is not set
CONFIG_NETDEVICES=y
# CONFIG_DUMMY is not set
# CONFIG_MACVLAN is not set
# CONFIG_EQUALIZER is not set
# CONFIG_TUN is not set
# CONFIG_VETH is not set
# CONFIG_NET_ETHERNET is not set
CONFIG_NETDEV_1000=y
CONFIG_NETDEV_10000=y

#
# Wireless LAN
#
# CONFIG_WLAN_PRE80211 is not set
# CONFIG_WLAN_80211 is not set

#
# Enable WiMAX (Networking options) to see the WiMAX drivers
#
# CONFIG_WAN is not set
# CONFIG_PPP is not set
# CONFIG_SLIP is not set
# CONFIG_NETCONSOLE is not set
# CONFIG_NETPOLL is not set
# CONFIG_NET_POLL_CONTROLLER is not set
# CONFIG_ISDN is not set

#
# Input device support
#
CONFIG_INPUT=y
# CONFIG_INPUT_FF_MEMLESS is not set
CONFIG_INPUT_POLLDEV=y

#
# Userland interfaces
#
# CONFIG_INPUT_MOUSEDEV is not set
# CONFIG_INPUT_JOYDEV is not set
CONFIG_INPUT_EVDEV=y
# CONFIG_INPUT_EVBUG is not set

#
# Input Device Drivers
#
CONFIG_INPUT_KEYBOARD=y
# CONFIG_KEYBOARD_ATKBD is not set
# CONFIG_KEYBOARD_LKKBD is not set
# CONFIG_KEYBOARD_GPIO is not set
# CONFIG_KEYBOARD_MATRIX is not set
# CONFIG_KEYBOARD_NEWTON is not set
# CONFIG_KEYBOARD_STOWAWAY is not set
# CONFIG_KEYBOARD_SUNKBD is not set
# CONFIG_KEYBOARD_XTKBD is not set
# CONFIG_KEYBOARD_MXC is not set
# CONFIG_KEYBOARD_MC9S08DZ60 is not set
# CONFIG_INPUT_MOUSE is not set
# CONFIG_INPUT_JOYSTICK is not set
# CONFIG_INPUT_TABLET is not set
# CONFIG_INPUT_TOUCHSCREEN is not set
# CONFIG_INPUT_MISC is not set

#
# Hardware I/O ports
#
# CONFIG_SERIO is not set
# CONFIG_GAMEPORT is not set

#
# Character devices
#
CONFIG_VT=y
CONFIG_CONSOLE_TRANSLATIONS=y
CONFIG_VT_CONSOLE=y
CONFIG_HW_CONSOLE=y
# CONFIG_VT_HW_CONSOLE_BINDING is not set
CONFIG_DEVKMEM=y
# CONFIG_SERIAL_NONSTANDARD is not set
CONFIG_FM_SI4702=m
CONFIG_MXC_IIM=y

#
# Serial drivers
#
# CONFIG_SERIAL_8250 is not set

#
# Non-8250 serial port support
#
CONFIG_SERIAL_MXC=y
CONFIG_SERIAL_MXC_CONSOLE=y
# CONFIG_SERIAL_MAX3100 is not set
# CONFIG_SERIAL_IMX is not set
CONFIG_SERIAL_CORE=y
CONFIG_SERIAL_CORE_CONSOLE=y
CONFIG_UNIX98_PTYS=y
# CONFIG_DEVPTS_MULTIPLE_INSTANCES is not set
CONFIG_LEGACY_PTYS=y
CONFIG_LEGACY_PTY_COUNT=256
# CONFIG_IPMI_HANDLER is not set
CONFIG_HW_RANDOM=y
# CONFIG_HW_RANDOM_TIMERIOMEM is not set
# CONFIG_HW_RANDOM_FSL_RNGC is not set
# CONFIG_R3964 is not set
# CONFIG_RAW_DRIVER is not set
# CONFIG_TCG_TPM is not set
CONFIG_I2C=y
CONFIG_I2C_BOARDINFO=y
CONFIG_I2C_CHARDEV=y
CONFIG_I2C_HELPER_AUTO=y

#
# I2C Hardware Bus support
#

#
# I2C system bus drivers (mostly embedded / system-on-chip)
#
# CONFIG_I2C_GPIO is not set
# CONFIG_I2C_IMX is not set
CONFIG_I2C_MXC=y
# CONFIG_I2C_MXC_HS is not set
# CONFIG_I2C_OCORES is not set
# CONFIG_I2C_SIMTEC is not set

#
# External I2C/SMBus adapter drivers
#
# CONFIG_I2C_PARPORT_LIGHT is not set
# CONFIG_I2C_TAOS_EVM is not set

#
# Other I2C/SMBus bus drivers
#
# CONFIG_I2C_PCA_PLATFORM is not set
# CONFIG_I2C_STUB is not set

#
# Miscellaneous I2C Chip support
#
# CONFIG_DS1682 is not set
# CONFIG_SENSORS_PCF8574 is not set
# CONFIG_PCF8575 is not set
# CONFIG_SENSORS_PCA9539 is not set
# CONFIG_SENSORS_TSL2550 is not set
# CONFIG_I2C_DEBUG_CORE is not set
# CONFIG_I2C_DEBUG_ALGO is not set
# CONFIG_I2C_DEBUG_BUS is not set
# CONFIG_I2C_DEBUG_CHIP is not set
# CONFIG_I2C_SLAVE is not set
CONFIG_SPI=y
# CONFIG_SPI_DEBUG is not set
CONFIG_SPI_MASTER=y

#
# SPI Master Controller Drivers
#
CONFIG_SPI_BITBANG=y
# CONFIG_SPI_GPIO is not set
CONFIG_SPI_MXC=y
# CONFIG_SPI_MXC_TEST_LOOPBACK is not set
CONFIG_SPI_MXC_SELECT1=y
# CONFIG_SPI_MXC_SELECT2 is not set

#
# SPI Protocol Masters
#
# CONFIG_SPI_SPIDEV is not set
# CONFIG_SPI_TLE62X0 is not set
CONFIG_ARCH_REQUIRE_GPIOLIB=y
CONFIG_GPIOLIB=y
# CONFIG_DEBUG_GPIO is not set
CONFIG_GPIO_SYSFS=y

#
# Memory mapped GPIO expanders:
#

#
# I2C GPIO expanders:
#
# CONFIG_GPIO_MAX732X is not set
# CONFIG_GPIO_PCA953X is not set
# CONFIG_GPIO_PCF857X is not set

#
# PCI GPIO expanders:
#

#
# SPI GPIO expanders:
#
# CONFIG_GPIO_MAX7301 is not set
# CONFIG_GPIO_MCP23S08 is not set
# CONFIG_W1 is not set
# CONFIG_POWER_SUPPLY is not set
# CONFIG_HWMON is not set
# CONFIG_THERMAL is not set
# CONFIG_THERMAL_HWMON is not set
CONFIG_WATCHDOG=y
CONFIG_WATCHDOG_NOWAYOUT=y

#
# Watchdog Device Drivers
#
# CONFIG_SOFT_WATCHDOG is not set
CONFIG_MXC_WATCHDOG=y
CONFIG_SSB_POSSIBLE=y

#
# Sonics Silicon Backplane
#
# CONFIG_SSB is not set

#
# Multifunction device drivers
#
# CONFIG_MFD_CORE is not set
# CONFIG_MFD_SM501 is not set
# CONFIG_MFD_ASIC3 is not set
# CONFIG_HTC_EGPIO is not set
# CONFIG_HTC_PASIC3 is not set
# CONFIG_TPS65010 is not set
# CONFIG_TWL4030_CORE is not set
# CONFIG_MFD_TMIO is not set
# CONFIG_MFD_TC6393XB is not set
# CONFIG_PMIC_DA903X is not set
# CONFIG_MFD_WM8400 is not set
# CONFIG_MFD_WM8350_I2C is not set
# CONFIG_MFD_PCF50633 is not set
# CONFIG_AB3100_CORE is not set
# CONFIG_EZX_PCAP is not set
CONFIG_MEDIA_SUPPORT=y

#
# Multimedia core support
#
CONFIG_VIDEO_DEV=y
CONFIG_VIDEO_V4L2_COMMON=y
CONFIG_VIDEO_ALLOW_V4L1=y
CONFIG_VIDEO_V4L1_COMPAT=y
CONFIG_VIDEO_MEDIA=y

#
# Multimedia drivers
#
# CONFIG_MEDIA_ATTACH is not set
CONFIG_MEDIA_TUNER=y
# CONFIG_MEDIA_TUNER_CUSTOMISE is not set
CONFIG_MEDIA_TUNER_SIMPLE=y
CONFIG_MEDIA_TUNER_TDA8290=y
CONFIG_MEDIA_TUNER_TDA9887=y
CONFIG_MEDIA_TUNER_TEA5761=y
CONFIG_MEDIA_TUNER_TEA5767=y
CONFIG_MEDIA_TUNER_MT20XX=y
CONFIG_MEDIA_TUNER_XC2028=y
CONFIG_MEDIA_TUNER_XC5000=y
CONFIG_MEDIA_TUNER_MC44S803=y
CONFIG_VIDEO_V4L2=y
CONFIG_VIDEO_V4L1=y
CONFIG_VIDEO_CAPTURE_DRIVERS=y
# CONFIG_VIDEO_ADV_DEBUG is not set
# CONFIG_VIDEO_FIXED_MINOR_RANGES is not set
# CONFIG_VIDEO_HELPER_CHIPS_AUTO is not set

#
# Encoders/decoders and other helper chips
#

#
# Audio decoders
#
# CONFIG_VIDEO_TVAUDIO is not set
# CONFIG_VIDEO_TDA7432 is not set
# CONFIG_VIDEO_TDA9840 is not set
# CONFIG_VIDEO_TDA9875 is not set
# CONFIG_VIDEO_TEA6415C is not set
# CONFIG_VIDEO_TEA6420 is not set
# CONFIG_VIDEO_MSP3400 is not set
# CONFIG_VIDEO_CS5345 is not set
# CONFIG_VIDEO_CS53L32A is not set
# CONFIG_VIDEO_M52790 is not set
# CONFIG_VIDEO_TLV320AIC23B is not set
# CONFIG_VIDEO_WM8775 is not set
# CONFIG_VIDEO_WM8739 is not set
# CONFIG_VIDEO_VP27SMPX is not set

#
# RDS decoders
#
# CONFIG_VIDEO_SAA6588 is not set

#
# Video decoders
#
# CONFIG_VIDEO_BT819 is not set
# CONFIG_VIDEO_BT856 is not set
# CONFIG_VIDEO_BT866 is not set
# CONFIG_VIDEO_KS0127 is not set
# CONFIG_VIDEO_OV7670 is not set
# CONFIG_VIDEO_MT9V011 is not set
# CONFIG_VIDEO_TCM825X is not set
# CONFIG_VIDEO_SAA7110 is not set
# CONFIG_VIDEO_SAA711X is not set
# CONFIG_VIDEO_SAA717X is not set
# CONFIG_VIDEO_SAA7191 is not set
# CONFIG_VIDEO_TVP514X is not set
# CONFIG_VIDEO_TVP5150 is not set
# CONFIG_VIDEO_VPX3220 is not set

#
# Video and audio decoders
#
# CONFIG_VIDEO_CX25840 is not set

#
# MPEG video encoders
#
# CONFIG_VIDEO_CX2341X is not set

#
# Video encoders
#
# CONFIG_VIDEO_SAA7127 is not set
# CONFIG_VIDEO_SAA7185 is not set
# CONFIG_VIDEO_ADV7170 is not set
# CONFIG_VIDEO_ADV7175 is not set
# CONFIG_VIDEO_THS7303 is not set
# CONFIG_VIDEO_ADV7343 is not set

#
# Video improvement chips
#
# CONFIG_VIDEO_UPD64031A is not set
# CONFIG_VIDEO_UPD64083 is not set
# CONFIG_VIDEO_VIVI is not set
# CONFIG_VIDEO_MXC_CAMERA is not set
CONFIG_VIDEO_MXC_OUTPUT=y
CONFIG_VIDEO_MXC_IPU_OUTPUT=y
# CONFIG_VIDEO_MXC_IPUV1_WVGA_OUTPUT is not set
# CONFIG_VIDEO_MXC_OPL is not set
# CONFIG_VIDEO_CPIA is not set
# CONFIG_VIDEO_SAA5246A is not set
# CONFIG_VIDEO_SAA5249 is not set
# CONFIG_SOC_CAMERA is not set
CONFIG_RADIO_ADAPTERS=y
# CONFIG_RADIO_TEA5764 is not set
# CONFIG_DAB is not set

#
# Graphics support
#
# CONFIG_VGASTATE is not set
# CONFIG_VIDEO_OUTPUT_CONTROL is not set
CONFIG_FB=y
# CONFIG_FIRMWARE_EDID is not set
# CONFIG_FB_DDC is not set
# CONFIG_FB_BOOT_VESA_SUPPORT is not set
CONFIG_FB_CFB_FILLRECT=y
CONFIG_FB_CFB_COPYAREA=y
CONFIG_FB_CFB_IMAGEBLIT=y
# CONFIG_FB_CFB_REV_PIXELS_IN_BYTE is not set
# CONFIG_FB_SYS_FILLRECT is not set
# CONFIG_FB_SYS_COPYAREA is not set
# CONFIG_FB_SYS_IMAGEBLIT is not set
# CONFIG_FB_FOREIGN_ENDIAN is not set
# CONFIG_FB_SYS_FOPS is not set
# CONFIG_FB_SVGALIB is not set
# CONFIG_FB_MACMODES is not set
# CONFIG_FB_BACKLIGHT is not set
CONFIG_FB_MODE_HELPERS=y
# CONFIG_FB_TILEBLITTING is not set

#
# Frame buffer hardware drivers
#
CONFIG_FB_MXC=y
CONFIG_FB_MXC_SYNC_PANEL=y
# CONFIG_FB_MXC_EPSON_VGA_SYNC_PANEL is not set
CONFIG_FB_MXC_CLAA_WVGA_SYNC_PANEL=y
# CONFIG_FB_MXC_CH7026 is not set
# CONFIG_FB_MXC_TVOUT_CH7024 is not set
# CONFIG_FB_MXC_ASYNC_PANEL is not set
# CONFIG_FB_S1D13XXX is not set
# CONFIG_FB_VIRTUAL is not set
# CONFIG_FB_METRONOME is not set
# CONFIG_FB_MB862XX is not set
# CONFIG_FB_BROADSHEET is not set
# CONFIG_BACKLIGHT_LCD_SUPPORT is not set

#
# Display device support
#
CONFIG_DISPLAY_SUPPORT=y

#
# Display hardware drivers
#

#
# Console display driver support
#
# CONFIG_VGA_CONSOLE is not set
CONFIG_DUMMY_CONSOLE=y
CONFIG_FRAMEBUFFER_CONSOLE=m
# CONFIG_FRAMEBUFFER_CONSOLE_DETECT_PRIMARY is not set
# CONFIG_FRAMEBUFFER_CONSOLE_ROTATION is not set
CONFIG_FONTS=y
# CONFIG_FONT_8x8 is not set
CONFIG_FONT_8x16=y
# CONFIG_FONT_6x11 is not set
# CONFIG_FONT_7x14 is not set
# CONFIG_FONT_PEARL_8x8 is not set
# CONFIG_FONT_ACORN_8x8 is not set
# CONFIG_FONT_MINI_4x6 is not set
# CONFIG_FONT_SUN8x16 is not set
# CONFIG_FONT_SUN12x22 is not set
# CONFIG_FONT_10x18 is not set
CONFIG_LOGO=y
CONFIG_LOGO_LINUX_MONO=y
CONFIG_LOGO_LINUX_VGA16=y
CONFIG_LOGO_LINUX_CLUT224=y
# CONFIG_SOUND is not set
CONFIG_HID_SUPPORT=y
CONFIG_HID=y
# CONFIG_HID_DEBUG is not set
# CONFIG_HIDRAW is not set
# CONFIG_HID_PID is not set

#
# Special HID drivers
#
CONFIG_USB_SUPPORT=y
CONFIG_USB_ARCH_HAS_HCD=y
# CONFIG_USB_ARCH_HAS_OHCI is not set
CONFIG_USB_ARCH_HAS_EHCI=y
# CONFIG_USB is not set
CONFIG_USB_OTG_WHITELIST=y
# CONFIG_USB_OTG_BLACKLIST_HUB is not set
# CONFIG_USB_GADGET_MUSB_HDRC is not set

#
# NOTE: USB_STORAGE depends on SCSI but BLK_DEV_SD may
#
CONFIG_USB_GADGET=y
# CONFIG_USB_GADGET_DEBUG is not set
# CONFIG_USB_GADGET_DEBUG_FILES is not set
# CONFIG_USB_GADGET_DEBUG_FS is not set
CONFIG_USB_GADGET_VBUS_DRAW=100
CONFIG_USB_GADGET_SELECTED=y
# CONFIG_USB_GADGET_AT91 is not set
# CONFIG_USB_GADGET_ATMEL_USBA is not set
CONFIG_USB_GADGET_FSL_USB2=y
CONFIG_USB_FSL_USB2=y
# CONFIG_USB_GADGET_LH7A40X is not set
# CONFIG_USB_GADGET_OMAP is not set
# CONFIG_USB_GADGET_PXA25X is not set
# CONFIG_USB_GADGET_PXA27X is not set
# CONFIG_USB_GADGET_S3C_HSOTG is not set
# CONFIG_USB_GADGET_IMX is not set
# CONFIG_USB_GADGET_S3C2410 is not set
# CONFIG_USB_GADGET_M66592 is not set
# CONFIG_USB_GADGET_AMD5536UDC is not set
# CONFIG_USB_GADGET_FSL_QE is not set
# CONFIG_USB_GADGET_CI13XXX is not set
# CONFIG_USB_GADGET_NET2280 is not set
# CONFIG_USB_GADGET_GOKU is not set
# CONFIG_USB_GADGET_ARC is not set
# CONFIG_USB_GADGET_LANGWELL is not set
# CONFIG_USB_GADGET_DUMMY_HCD is not set
CONFIG_USB_GADGET_DUALSPEED=y
# CONFIG_USB_ZERO is not set
# CONFIG_USB_AUDIO is not set
# CONFIG_USB_ETH is not set
# CONFIG_USB_GADGETFS is not set
CONFIG_USB_FILE_STORAGE=y
# CONFIG_USB_FILE_STORAGE_TEST is not set
# CONFIG_USB_G_SERIAL is not set
# CONFIG_USB_MIDI_GADGET is not set
# CONFIG_USB_G_PRINTER is not set
# CONFIG_USB_CDC_COMPOSITE is not set

#
# OTG and related infrastructure
#
# CONFIG_USB_GPIO_VBUS is not set
# CONFIG_NOP_USB_XCEIV is not set
CONFIG_MMC=y
# CONFIG_MMC_DEBUG is not set
CONFIG_MMC_UNSAFE_RESUME=y

#
# MMC/SD/SDIO Card Drivers
#
CONFIG_MMC_BLOCK=y
CONFIG_MMC_BLOCK_BOUNCE=y
# CONFIG_SDIO_UART is not set
# CONFIG_MMC_TEST is not set
CONFIG_SDIO_UNIFI_FS=m

#
# MMC/SD/SDIO Host Controller Drivers
#
# CONFIG_MMC_SDHCI is not set
# CONFIG_MMC_MXC is not set
# CONFIG_MMC_SPI is not set
CONFIG_MMC_IMX_ESDHCI=m
# CONFIG_MMC_IMX_ESDHCI_PIO_MODE is not set
# CONFIG_MEMSTICK is not set
# CONFIG_ACCESSIBILITY is not set
# CONFIG_NEW_LEDS is not set
CONFIG_RTC_LIB=y
CONFIG_RTC_CLASS=y
CONFIG_RTC_HCTOSYS=y
CONFIG_RTC_HCTOSYS_DEVICE="rtc0"
# CONFIG_RTC_DEBUG is not set

#
# RTC interfaces
#
CONFIG_RTC_INTF_SYSFS=y
CONFIG_RTC_INTF_PROC=y
CONFIG_RTC_INTF_DEV=y
# CONFIG_RTC_INTF_DEV_UIE_EMUL is not set
# CONFIG_RTC_DRV_TEST is not set

#
# I2C RTC drivers
#
# CONFIG_RTC_DRV_DS1307 is not set
# CONFIG_RTC_DRV_DS1374 is not set
# CONFIG_RTC_DRV_DS1672 is not set
# CONFIG_RTC_DRV_MAX6900 is not set
# CONFIG_RTC_DRV_RS5C372 is not set
# CONFIG_RTC_DRV_ISL1208 is not set
# CONFIG_RTC_DRV_X1205 is not set
# CONFIG_RTC_DRV_PCF8563 is not set
# CONFIG_RTC_DRV_PCF8583 is not set
# CONFIG_RTC_DRV_M41T80 is not set
# CONFIG_RTC_DRV_S35390A is not set
# CONFIG_RTC_DRV_FM3130 is not set
# CONFIG_RTC_DRV_RX8581 is not set
# CONFIG_RTC_DRV_RX8025 is not set

#
# SPI RTC drivers
#
# CONFIG_RTC_DRV_M41T94 is not set
# CONFIG_RTC_DRV_DS1305 is not set
# CONFIG_RTC_DRV_DS1390 is not set
# CONFIG_RTC_DRV_MAX6902 is not set
# CONFIG_RTC_DRV_R9701 is not set
# CONFIG_RTC_DRV_RS5C348 is not set
# CONFIG_RTC_DRV_DS3234 is not set

#
# Platform RTC drivers
#
# CONFIG_RTC_DRV_CMOS is not set
# CONFIG_RTC_DRV_DS1286 is not set
# CONFIG_RTC_DRV_DS1511 is not set
# CONFIG_RTC_DRV_DS1553 is not set
# CONFIG_RTC_DRV_DS1742 is not set
# CONFIG_RTC_DRV_STK17TA8 is not set
# CONFIG_RTC_DRV_M48T86 is not set
# CONFIG_RTC_DRV_M48T35 is not set
# CONFIG_RTC_DRV_M48T59 is not set
# CONFIG_RTC_DRV_BQ4802 is not set
# CONFIG_RTC_DRV_V3020 is not set

#
# on-CPU RTC drivers
#
CONFIG_RTC_MXC=y
# CONFIG_RTC_DRV_MXC_V2 is not set
# CONFIG_RTC_DRV_IMXDI is not set
CONFIG_RTC_MC13892=y
CONFIG_DMADEVICES=y

#
# DMA Devices
#
# CONFIG_AUXDISPLAY is not set
CONFIG_REGULATOR=y
# CONFIG_REGULATOR_DEBUG is not set
# CONFIG_REGULATOR_FIXED_VOLTAGE is not set
# CONFIG_REGULATOR_VIRTUAL_CONSUMER is not set
# CONFIG_REGULATOR_USERSPACE_CONSUMER is not set
# CONFIG_REGULATOR_BQ24022 is not set
# CONFIG_REGULATOR_MAX1586 is not set
# CONFIG_REGULATOR_LP3971 is not set
CONFIG_REGULATOR_MC13892=y
CONFIG_REGULATOR_MC9S08DZ60=y
# CONFIG_UIO is not set
# CONFIG_STAGING is not set

#
# MXC support drivers
#
CONFIG_MXC_IPU=y
CONFIG_MXC_IPU_V1=y
CONFIG_MXC_IPU_PF=y

#
# MXC SSI support
#
# CONFIG_MXC_SSI is not set

#
# MXC Digital Audio Multiplexer support
#
# CONFIG_MXC_DAM is not set

#
# MXC PMIC support
#
CONFIG_MXC_PMIC=y
# CONFIG_MXC_PMIC_MC13783 is not set
CONFIG_MXC_PMIC_MC13892=y
CONFIG_MXC_PMIC_I2C=y
# CONFIG_MXC_PMIC_SPI is not set
# CONFIG_MXC_PMIC_MC34704 is not set
CONFIG_MXC_PMIC_MC9SDZ60=y
# CONFIG_MXC_PMIC_CHARDEV is not set

#
# MXC PMIC Client Drivers
#
CONFIG_MXC_MC13892_ADC=y
CONFIG_MXC_MC13892_RTC=y
CONFIG_MXC_MC13892_LIGHT=y
# CONFIG_MXC_MC13892_BATTERY is not set
# CONFIG_MXC_MC13892_CONNECTIVITY is not set
CONFIG_MXC_MC13892_POWER=y
CONFIG_MXC_PMIC_MC9S08DZ60=y
# CONFIG_MXC_MC9SDZ60_RTC is not set

#
# MXC Security Drivers
#
CONFIG_MXC_SECURITY_SCC=y
# CONFIG_SCC_DEBUG is not set
# CONFIG_MXC_SECURITY_RNG is not set

#
# MXC MPEG4 Encoder Kernel module support
#
# CONFIG_MXC_HMP4E is not set

#
# MXC HARDWARE EVENT
#
# CONFIG_MXC_HWEVENT is not set

#
# MXC VPU(Video Processing Unit) support
#

#
# MXC Asynchronous Sample Rate Converter support
#
CONFIG_MXC_ASRC=y

#
# MXC Bluetooth support
#
CONFIG_MXC_BLUETOOTH=m

#
# Broadcom GPS ioctrl support
#
CONFIG_GPS_IOCTRL=m

#
# MXC Media Local Bus Driver
#
CONFIG_MXC_MLB=m

#
# i.MX ADC support
#
# CONFIG_IMX_ADC is not set

#
# File systems
#
CONFIG_EXT2_FS=y
# CONFIG_EXT2_FS_XATTR is not set
# CONFIG_EXT2_FS_XIP is not set
# CONFIG_EXT3_FS is not set
# CONFIG_EXT4_FS is not set
# CONFIG_REISERFS_FS is not set
# CONFIG_JFS_FS is not set
# CONFIG_FS_POSIX_ACL is not set
# CONFIG_XFS_FS is not set
# CONFIG_GFS2_FS is not set
# CONFIG_OCFS2_FS is not set
# CONFIG_BTRFS_FS is not set
CONFIG_FILE_LOCKING=y
CONFIG_FSNOTIFY=y
CONFIG_DNOTIFY=y
CONFIG_INOTIFY=y
CONFIG_INOTIFY_USER=y
# CONFIG_QUOTA is not set
# CONFIG_AUTOFS_FS is not set
CONFIG_AUTOFS4_FS=m
# CONFIG_FUSE_FS is not set

#
# Caches
#
# CONFIG_FSCACHE is not set

#
# CD-ROM/DVD Filesystems
#
CONFIG_ISO9660_FS=y
CONFIG_JOLIET=y
CONFIG_ZISOFS=y
# CONFIG_UDF_FS is not set

#
# DOS/FAT/NT Filesystems
#
CONFIG_FAT_FS=y
CONFIG_MSDOS_FS=y
CONFIG_VFAT_FS=y
CONFIG_FAT_DEFAULT_CODEPAGE=437
CONFIG_FAT_DEFAULT_IOCHARSET="iso8859-1"
# CONFIG_NTFS_FS is not set

#
# Pseudo filesystems
#
CONFIG_PROC_FS=y
CONFIG_PROC_SYSCTL=y
CONFIG_PROC_PAGE_MONITOR=y
CONFIG_SYSFS=y
CONFIG_TMPFS=y
# CONFIG_TMPFS_POSIX_ACL is not set
# CONFIG_HUGETLB_PAGE is not set
# CONFIG_CONFIGFS_FS is not set
CONFIG_MISC_FILESYSTEMS=y
# CONFIG_ADFS_FS is not set
# CONFIG_AFFS_FS is not set
# CONFIG_HFS_FS is not set
# CONFIG_HFSPLUS_FS is not set
# CONFIG_BEFS_FS is not set
# CONFIG_BFS_FS is not set
# CONFIG_EFS_FS is not set
# CONFIG_JFFS2_FS is not set
CONFIG_CRAMFS=y
# CONFIG_SQUASHFS is not set
# CONFIG_VXFS_FS is not set
# CONFIG_MINIX_FS is not set
# CONFIG_OMFS_FS is not set
# CONFIG_HPFS_FS is not set
# CONFIG_QNX4FS_FS is not set
# CONFIG_ROMFS_FS is not set
# CONFIG_SYSV_FS is not set
# CONFIG_UFS_FS is not set
# CONFIG_NILFS2_FS is not set
CONFIG_NETWORK_FILESYSTEMS=y

#
# Partition Types
#
# CONFIG_PARTITION_ADVANCED is not set
CONFIG_MSDOS_PARTITION=y
CONFIG_NLS=y
CONFIG_NLS_DEFAULT="iso8859-1"
CONFIG_NLS_CODEPAGE_437=y
# CONFIG_NLS_CODEPAGE_737 is not set
# CONFIG_NLS_CODEPAGE_775 is not set
# CONFIG_NLS_CODEPAGE_850 is not set
# CONFIG_NLS_CODEPAGE_852 is not set
# CONFIG_NLS_CODEPAGE_855 is not set
# CONFIG_NLS_CODEPAGE_857 is not set
# CONFIG_NLS_CODEPAGE_860 is not set
# CONFIG_NLS_CODEPAGE_861 is not set
# CONFIG_NLS_CODEPAGE_862 is not set
# CONFIG_NLS_CODEPAGE_863 is not set
# CONFIG_NLS_CODEPAGE_864 is not set
# CONFIG_NLS_CODEPAGE_865 is not set
# CONFIG_NLS_CODEPAGE_866 is not set
# CONFIG_NLS_CODEPAGE_869 is not set
# CONFIG_NLS_CODEPAGE_936 is not set
# CONFIG_NLS_CODEPAGE_950 is not set
# CONFIG_NLS_CODEPAGE_932 is not set
# CONFIG_NLS_CODEPAGE_949 is not set
# CONFIG_NLS_CODEPAGE_874 is not set
# CONFIG_NLS_ISO8859_8 is not set
# CONFIG_NLS_CODEPAGE_1250 is not set
# CONFIG_NLS_CODEPAGE_1251 is not set
CONFIG_NLS_ASCII=m
CONFIG_NLS_ISO8859_1=y
# CONFIG_NLS_ISO8859_2 is not set
# CONFIG_NLS_ISO8859_3 is not set
# CONFIG_NLS_ISO8859_4 is not set
# CONFIG_NLS_ISO8859_5 is not set
# CONFIG_NLS_ISO8859_6 is not set
# CONFIG_NLS_ISO8859_7 is not set
# CONFIG_NLS_ISO8859_9 is not set
# CONFIG_NLS_ISO8859_13 is not set
# CONFIG_NLS_ISO8859_14 is not set
# CONFIG_NLS_ISO8859_15 is not set
# CONFIG_NLS_KOI8_R is not set
# CONFIG_NLS_KOI8_U is not set
CONFIG_NLS_UTF8=m

#
# Kernel hacking
#
# CONFIG_PRINTK_TIME is not set
CONFIG_ENABLE_WARN_DEPRECATED=y
CONFIG_ENABLE_MUST_CHECK=y
CONFIG_FRAME_WARN=1024
CONFIG_MAGIC_SYSRQ=y
# CONFIG_UNUSED_SYMBOLS is not set
CONFIG_DEBUG_FS=y
# CONFIG_HEADERS_CHECK is not set
CONFIG_DEBUG_KERNEL=y
# CONFIG_DEBUG_SHIRQ is not set
CONFIG_DETECT_SOFTLOCKUP=y
# CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC is not set
CONFIG_BOOTPARAM_SOFTLOCKUP_PANIC_VALUE=0
CONFIG_DETECT_HUNG_TASK=y
# CONFIG_BOOTPARAM_HUNG_TASK_PANIC is not set
CONFIG_BOOTPARAM_HUNG_TASK_PANIC_VALUE=0
CONFIG_SCHED_DEBUG=y
# CONFIG_SCHEDSTATS is not set
# CONFIG_TIMER_STATS is not set
# CONFIG_DEBUG_OBJECTS is not set
# CONFIG_SLUB_DEBUG_ON is not set
# CONFIG_SLUB_STATS is not set
# CONFIG_DEBUG_KMEMLEAK is not set
CONFIG_DEBUG_PREEMPT=y
# CONFIG_DEBUG_RT_MUTEXES is not set
# CONFIG_RT_MUTEX_TESTER is not set
# CONFIG_DEBUG_SPINLOCK is not set
# CONFIG_DEBUG_MUTEXES is not set
# CONFIG_DEBUG_LOCK_ALLOC is not set
# CONFIG_PROVE_LOCKING is not set
# CONFIG_LOCK_STAT is not set
# CONFIG_DEBUG_SPINLOCK_SLEEP is not set
# CONFIG_DEBUG_LOCKING_API_SELFTESTS is not set
CONFIG_STACKTRACE=y
# CONFIG_DEBUG_KOBJECT is not set
# CONFIG_DEBUG_BUGVERBOSE is not set
CONFIG_DEBUG_INFO=y
# CONFIG_DEBUG_VM is not set
# CONFIG_DEBUG_WRITECOUNT is not set
# CONFIG_DEBUG_MEMORY_INIT is not set
# CONFIG_DEBUG_LIST is not set
# CONFIG_DEBUG_SG is not set
# CONFIG_DEBUG_NOTIFIERS is not set
# CONFIG_BOOT_PRINTK_DELAY is not set
# CONFIG_RCU_TORTURE_TEST is not set
# CONFIG_RCU_CPU_STALL_DETECTOR is not set
# CONFIG_BACKTRACE_SELF_TEST is not set
# CONFIG_DEBUG_BLOCK_EXT_DEVT is not set
# CONFIG_FAULT_INJECTION is not set
# CONFIG_LATENCYTOP is not set
CONFIG_SYSCTL_SYSCALL_CHECK=y
# CONFIG_PAGE_POISONING is not set
CONFIG_NOP_TRACER=y
CONFIG_HAVE_FUNCTION_TRACER=y
CONFIG_RING_BUFFER=y
CONFIG_EVENT_TRACING=y
CONFIG_CONTEXT_SWITCH_TRACER=y
CONFIG_TRACING=y
CONFIG_TRACING_SUPPORT=y
# CONFIG_FTRACE is not set
# CONFIG_DYNAMIC_DEBUG is not set
# CONFIG_SAMPLES is not set
CONFIG_HAVE_ARCH_KGDB=y
# CONFIG_KGDB is not set
CONFIG_ARM_UNWIND=y
# CONFIG_DEBUG_USER is not set
# CONFIG_DEBUG_ERRORS is not set
# CONFIG_DEBUG_STACK_USAGE is not set
CONFIG_DEBUG_LL=y
# CONFIG_DEBUG_ICEDCC is not set

#
# Security options
#
# CONFIG_KEYS is not set
# CONFIG_SECURITY is not set
# CONFIG_SECURITYFS is not set
# CONFIG_SECURITY_FILE_CAPABILITIES is not set
CONFIG_CRYPTO=y

#
# Crypto core or helper
#
# CONFIG_CRYPTO_FIPS is not set
# CONFIG_CRYPTO_MANAGER is not set
# CONFIG_CRYPTO_MANAGER2 is not set
# CONFIG_CRYPTO_GF128MUL is not set
# CONFIG_CRYPTO_NULL is not set
# CONFIG_CRYPTO_CRYPTD is not set
# CONFIG_CRYPTO_AUTHENC is not set
# CONFIG_CRYPTO_TEST is not set
# CONFIG_CRYPTO_CRYPTODEV is not set

#
# Authenticated Encryption with Associated Data
#
# CONFIG_CRYPTO_CCM is not set
# CONFIG_CRYPTO_GCM is not set
# CONFIG_CRYPTO_SEQIV is not set

#
# Block modes
#
# CONFIG_CRYPTO_CBC is not set
# CONFIG_CRYPTO_CTR is not set
# CONFIG_CRYPTO_CTS is not set
# CONFIG_CRYPTO_ECB is not set
# CONFIG_CRYPTO_LRW is not set
# CONFIG_CRYPTO_PCBC is not set
# CONFIG_CRYPTO_XTS is not set

#
# Hash modes
#
# CONFIG_CRYPTO_HMAC is not set
# CONFIG_CRYPTO_XCBC is not set

#
# Digest
#
# CONFIG_CRYPTO_CRC32C is not set
# CONFIG_CRYPTO_MD4 is not set
# CONFIG_CRYPTO_MD5 is not set
# CONFIG_CRYPTO_MICHAEL_MIC is not set
# CONFIG_CRYPTO_RMD128 is not set
# CONFIG_CRYPTO_RMD160 is not set
# CONFIG_CRYPTO_RMD256 is not set
# CONFIG_CRYPTO_RMD320 is not set
# CONFIG_CRYPTO_SHA1 is not set
# CONFIG_CRYPTO_SHA256 is not set
# CONFIG_CRYPTO_SHA512 is not set
# CONFIG_CRYPTO_TGR192 is not set
# CONFIG_CRYPTO_WP512 is not set

#
# Ciphers
#
# CONFIG_CRYPTO_AES is not set
# CONFIG_CRYPTO_ANUBIS is not set
# CONFIG_CRYPTO_ARC4 is not set
# CONFIG_CRYPTO_BLOWFISH is not set
# CONFIG_CRYPTO_CAMELLIA is not set
# CONFIG_CRYPTO_CAST5 is not set
# CONFIG_CRYPTO_CAST6 is not set
# CONFIG_CRYPTO_DES is not set
# CONFIG_CRYPTO_FCRYPT is not set
# CONFIG_CRYPTO_KHAZAD is not set
# CONFIG_CRYPTO_SALSA20 is not set
# CONFIG_CRYPTO_SEED is not set
# CONFIG_CRYPTO_SERPENT is not set
# CONFIG_CRYPTO_TEA is not set
# CONFIG_CRYPTO_TWOFISH is not set

#
# Compression
#
# CONFIG_CRYPTO_DEFLATE is not set
# CONFIG_CRYPTO_ZLIB is not set
# CONFIG_CRYPTO_LZO is not set

#
# Random Number Generation
#
# CONFIG_CRYPTO_ANSI_CPRNG is not set
CONFIG_CRYPTO_HW=y
CONFIG_BINARY_PRINTF=y

#
# Library routines
#
CONFIG_BITREVERSE=y
CONFIG_GENERIC_FIND_LAST_BIT=y
CONFIG_CRC_CCITT=m
# CONFIG_CRC16 is not set
# CONFIG_CRC_T10DIF is not set
# CONFIG_CRC_ITU_T is not set
CONFIG_CRC32=y
# CONFIG_CRC7 is not set
# CONFIG_LIBCRC32C is not set
CONFIG_ZLIB_INFLATE=y
CONFIG_DECOMPRESS_GZIP=y
CONFIG_HAS_IOMEM=y
CONFIG_HAS_IOPORT=y
CONFIG_HAS_DMA=y
CONFIG_NLATTR=y

Regards

Benoy

Labels (1)
0 Kudos
Reply
1 Solution
1,830 Views
benoysaha
Contributor II

Hello,

I could fix this issue after making couple of changes in .config .

Here is the details -

Device Drivers  --->

  [*] USB support  --->

    <*>   USB Gadget Support  --->

      (2)   Maximum VBUS Power usage (2-500 mA)

      USB Peripheral Controller (Freescale USB Device Controller)  --->

        Freescale USB Device Controller

      [*]   Support for DR peripheral port on Freescale controller

     Select transceiver for DR port (On-chip UTMI)  --->

        (X) On-chip UTMI

      [*]   OTG Support

Now it is working fine and i could detect my board as USB device from host PC.

Regards

Benoy

View solution in original post

0 Kudos
Reply
3 Replies
1,830 Views
fabio_estevam
NXP Employee
NXP Employee

I would suggest you to try with a more recent kernel, such as 3.8.

0 Kudos
Reply
1,831 Views
benoysaha
Contributor II

Hello,

I could fix this issue after making couple of changes in .config .

Here is the details -

Device Drivers  --->

  [*] USB support  --->

    <*>   USB Gadget Support  --->

      (2)   Maximum VBUS Power usage (2-500 mA)

      USB Peripheral Controller (Freescale USB Device Controller)  --->

        Freescale USB Device Controller

      [*]   Support for DR peripheral port on Freescale controller

     Select transceiver for DR port (On-chip UTMI)  --->

        (X) On-chip UTMI

      [*]   OTG Support

Now it is working fine and i could detect my board as USB device from host PC.

Regards

Benoy

0 Kudos
Reply
1,830 Views
eladshulman
Contributor II

Someone know what settings should I set for imx6q device ?

0 Kudos
Reply