IMX287 Power on Fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

IMX287 Power on Fail

2,625 次查看
nwpuxhy
Contributor I

     I designed a product  using iMX287 as MCU.Most of the time  the product work normal,sometimes the product does not work with boot fail . The probability is one in dozens.  In this abnormal condition ,the device will continuously ‘died’ until turn off the 5V power and turn on it.  I found the VDDIO drop down to 3.1V, VDDD drop down to 1.05V and VDDA drop down to 1.04V.I don't know why this happened, and I also don't know in which condition this will happen. How can I solve this problem?  Is there some problem with my schematic?  I use 5V only  source .

Best regards.I

标签 (1)
0 项奖励
回复
2 回复数

2,539 次查看
igorpadykov
NXP Employee
NXP Employee

Hi 许辉勇 许 

may be useful to look on

Brown out issues on ConnectCard (Wi)i.mx28 modules | Digi International 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,539 次查看
nwpuxhy
Contributor I

It.s not same with that.When the  iMX287 boot failed,the device will continuously ‘died’ until turn off the 5V power and turn on it.At the same time,the VDDIO drop down to 3.1V, VDDD drop down to 1.05V and VDDA drop down to 1.04V.

0 项奖励
回复