IMX28 reset due to VDDXTAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX28 reset due to VDDXTAL

Jump to solution
1,031 Views
djcatter
Contributor I

Based a design off of the reference board. We used the reference design power switch circuit to get us the two events. One is a button connected straight to VDDXTAL, the other is to the a 3.3V supply through a 10k resistor. We found an edge case where both events can occur and over drive VDDXTAL sometimes causing a reset. Yellow is the PSWITCH, pink is the VDDXTAL:

print_27.bmp
Now hindsight, I should have had a diode in place to block the 3.3V to the VDDXTAL. What I would like to know is where is the reset occuring? I have not been able to find it in the documentation where this reset is caused.

Thanks,

Derek

Labels (1)
Tags (2)
0 Kudos
Reply
1 Solution
680 Views
art
NXP Employee
NXP Employee

Since VDDXTAL supplies power to the main clock source oscillator, its overvoltage/undervoltage may break a stable clock generation, therefore, causing the reset to the whole system.

View solution in original post

0 Kudos
Reply
1 Reply
681 Views
art
NXP Employee
NXP Employee

Since VDDXTAL supplies power to the main clock source oscillator, its overvoltage/undervoltage may break a stable clock generation, therefore, causing the reset to the whole system.

0 Kudos
Reply