IMX28 DCDC_VDD unused

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX28 DCDC_VDD unused

Jump to solution
659 Views
dgotfroi
Contributor IV

Hello everybody,

I desgin a board with an IMX28 and I only use 3V3 and 1V8 from the IMX power supply. I didn't use VDD1P5 neither VDDD.

So, how can I connect VDD1P5 ? Can I leave it unconnected without capacitors or do I need to connect it to capacitors (10n, 100n 1u, 10u and 25u) ?

And what about VDDDx and DCDC_VDDD :

- Can I leave them unconnected ?

- Do I need to connect them together but without capacitors ?

- Or do I need to connect them together and with capacitors ?

This is my current schematic :

Capture.JPG.jpg

Do I need C1-C5 and C14-C21 ?

Many thanks for your help.

Labels (1)
Tags (3)
0 Kudos
1 Solution
521 Views
igorpadykov
NXP Employee
NXP Employee

Hi Damien

VDDD can not be left unconnected.

VDDD provides power to the digital core such as CPU and clocks,

as described in application note AN4199 (Rev.1 , 03/2013)

"Using the i.MX28 Power Management Unit and Battery Charger".

http://www.freescale.com/files/dsp/doc/app_note/AN4199.pdf

VDD1P5 can be left unconnected, if unused.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
2 Replies
522 Views
igorpadykov
NXP Employee
NXP Employee

Hi Damien

VDDD can not be left unconnected.

VDDD provides power to the digital core such as CPU and clocks,

as described in application note AN4199 (Rev.1 , 03/2013)

"Using the i.MX28 Power Management Unit and Battery Charger".

http://www.freescale.com/files/dsp/doc/app_note/AN4199.pdf

VDD1P5 can be left unconnected, if unused.

Best regards

chip

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 Kudos
521 Views
dgotfroi
Contributor IV

Hello,

Many thanks for your answer.

So, I will remove C1 to C5 and leave VDD1P5 unconnected.

It answers my question.

Thank you

0 Kudos